IAR Embedded Workbench for Renesas RL78

完全統合型開発ツールチェーンであるルネサス社製RL78用IAR Embedded Workbenchを使えば、1つのビューに1つのツールボックスが提供され、シームレスな1本のワークフローが可能です。

01

ユーザフレンドリなIDE

プロジェクト管理ツールとエディタを備えた統合開発環境です。リンカおよびライブラリツール、すべてのRL78ファミリデバイスのコンフィギュレーションファイル、サンプルプロジェクトおよびコードテンプレート、完全統合されたC-STAT静的解析が含まれています。

02

パワフルなビルドツール

高度な最適化を実現するRL78用C/C++コンパイラを備えています。RL78用再配置アセンブラ、ランタイムライブラリも有しています。

03

包括的なデバッガ

C-SPYデバッガはRL78用シミュレータを備えた包括的なデバッガです。ハードウェア上でのRTOS認識デバッグをサポートし、各種エミュレータに対応します。

04

統合化されたコード解析

IAR Embedded Workbench for RL78では、アドオンC-STATによる統合型の静的コード解析が可能です。これにより、MISRA C:2012などの規格との整合を確保するだけでなく、コード品質も向上させることができます。

最新リリースノート

弊社は、新しいデバイスのサポート、機能追加、および拡張など、ツールを常に更新し、向上に努めています。

Latest release: 5.10.3

  • The Renesas RL78/G24 Flexible Application Accelerator (FAA) co-processor is supported

    • The Renesas FAA assembler is incorporated in the IAR Embedded Workbench
    • FAA assembler-generated output is linked with the IAR linker
    • The IAR C-SPY debugger supports multicore debugging for the FAA core
  • Improved compliance with the CC-RL ABI specification

    Additional standard library functions and runtime routines have been implemented.
  • Debugging support for flash self-programming

    Debugging support while self-programming is in progress has been added for G2x and F2x devices.
  • Program corrections

    Errors have been corrected in the compiler, linker, and in IAR C-STAT.
Read complete release notes

Version: 5.10

  • Library support for the C++17 language standard
    The toolset includes a new C++ library that supports C++17 library features. 
  • Additional GNU C language extensions
    The IAR C/C++ Compiler supports a number of new GCC-style operators, attributes and expressions in extended language mode. 
  • Editor and IDE enhancements
    • Editor themes - a new way to set up the colors and fonts in the text editor
    • Syntax feedback - instant syntax suggestions while typing
    • Improved parameter hints
    • Window color themes - dark mode
    • Gray out inactive code support
  • Iarbuild enhancements
    The iarbuild command line build utility now supports:
    • Generating a Ninja build file based on the IAR Embedded Workbench project format
    • Generating a JSON description of the Embedded Workbench project
    • More C-STAT reporting and configuration methods
  • 64-bit Windows application
    IAR Embedded Workbench now runs as a 64-bit Windows application.
  • Visual Studio Code support
    The IAR Build and IAR C-SPY Debug extensions available on Microsoft Marketplace enable you to work in Visual Studio Code (with IAR Embedded Workbench installed) to:
    • Build IAR Embedded Workbench projects
    • Run the C-STAT static analysis tool
    • Debug applications using the same range of hardware/debug probes as in IAR Embedded Workbench. (An initial debug session with IAR Embedded Workbench is required to fill in the settings in the Hardware setup dialog box, prior to debugging in Visual Studio Code)
  • C-STAT enhancements
    • MISRA C:2012 Amendment 1
      The static analysis tool C-STAT has extended its coverage of the MISRA C:2012 Coding Standard and now fully supports MISRA C:2012 Amendment 1. This amendment adds 14 additional rules to MISRA C:2012 with a focus on security concerns highlighted by the ISO C Secure Guidelines. Several of these address specific issues pertaining to the use of untrustworthy data, a well-known security vulnerability.
    • MISRA C:2012 Amendment 2

      The static analysis tool C-STAT has extended its coverage of the MISRA C:2012 Coding Standard and now fully supports MISRA C:2012 Amendment 2. This Amendment adds two additional rules to MISRA C:2012 and introduces support for ISO/IEC 9899:2011, commonly referred to as "C11".

    • Improved performance
      Depending on the project, the analysis can be up to 40% faster and memory consumption reduced by up to 20%, compared to the previous version of C-STAT.
  • Updated device support
    The device support files have been updated to the most recent version from Renesas.
  • Updated user documentation
    The C/C++ Development Guide, C-SPY Debugging Guide, and IDE Project Management and Building Guide have been updated to reflect the product changes.
Read complete release notes

Version 4.21

  • RL78/G23 microcontroller group support
    The RL78/G23 group of microcontrollers is now supported.
  • IAR Build Tools for Linux
    A new product, IAR Build Tools for Renesas RL78, is available. It requires a separate product license and is distributed as a Debian package for Ubuntu containing the IAR C/C++ Compiler, IAR Assembler, Linker and library tools, C-STAT, IARBuild, and runtime libraries. Get product info
  • C-STAT enhancements
    • Extended coverage of CERT C
      The static analysis tool C-STAT has extended its coverage of the SEI CERT C Coding Standard. The SEI CERT C Coding Standard's goal is to provide rules for developing safe, reliable, and secure systems in the C programming language, with support for C11 constructs. C-STAT covers all rules in the different CERT C sections listed on the CERT C wiki as of January 2020, with the exception of the API, CON, POS, and WIN sections, which are not applicable to IAR Systems products, yielding a total of 90 covered rules.
    • Link analysis trace information
      The link analysis messages now display trace information when relevant. For checks looking for conflicting symbol names, all conflicting declarations are now listed in the trace information instead of each pair of conflicts being described in a separate message. This might lead to fewer reported messages for the same number of found issues.
  • Renesas Smart Configurator included
    The Renesas RL78 Smart Configurator V1.0.1 has been included.
Read complete release notes

Version 4.20

C18 support
The default Standard C is now C18 (ISO/IEC 9899:2018).

C++17 support
The compiler now supports almost all C++17 features. The C++ library supports C++14 with no C++17 additions.

Improved Source Browser
The following improvements have been made to the Source Browser:

    • The source browser data is generated faster as it is now running as a separate thread.
    • New Source Browser Log window.
    • Status indicator in the status bar.
    • Enhanced feedback in case source browsing data cannot be generated.

EZ-CUBE2 On-Chip Debug Emulator support
The EZ-CUBE2 On-Chip Debug Emulator, primarily targeted for the Chinese market, is now supported.

E2 emulator power debugging in C-SPY
The E2 emulator allows you to measure the dynamically changing current drawn by the user system. This is visualized as a graph in the C-SPY Timeline window as well as a list of time-current value pairs in the Power Log window. It is also possible to stop execution when the current goes above or below a certain user-defined threshold value.

Documentation Comments support in the editor
The editor can distinguish comments that start with /**, /*!, /// or //! as Documentation Comments. Inside a Documentation Comment, the editor can recognize keywords that begin with \ or @. If the keyword is recognized as a doxygen keyword, the Documentation Comment will appear in tooltips and parameter hints for variables and functions. See IAR Embedded Workbench IDE Project Management and Building Guide for more information.

Updated user documentation
The IDE Project Management and Building GuideC-SPY Debugging Guide and C/C++ Development Guide have been updated to reflect the product changes.

Read complete release notes

MCUデバイスを幅広くサポート

サポートされている RL78 デバイス

IAR Embedded Workbench for Renesas RL78を使用することで、Renesas RL78 MCUの機能を最大限に活用できます。

サポートされているデバイス一覧
renesas-rl78_supporteddevices2.png

どのようなタイプのライセンスが必要ですか?

IARシステムズのツールは、お客様の使用状況に応じて柔軟なライセンスモデルを用意しています。保守契約を締結されている場合は、世界中のどの地域でもサポートが受けられます。日本国内のユーザー様から日本法人へのお問い合わせについては、もちろん日本語のサポートが可能となります。 ご不明な点については、お気軽にお問い合わせよりご質問ください。

ライセンス情報の詳細はこちら

製品の詳細をお知りになりたいですか?

グローバルに展開するIARが世界各地のお客様をサポートします。製品に関するお問い合せには、常時お答えしています。

製品/見積もりに関する問い合わせ

製品に関するお問い合わせや見積もりのご依頼は、以下のフォームに必要事項をご記入の上、送信ボタンをクリックしてください。 *は必須項目となっています

* Privacy policy を確認

ベンチマーク結果

IAR Embedded Workbench for RL78の高度な最適化テクノロジにより、非常にコンパクトなコードが生成されます。

コードサイズのベンチマークテスト 

本ベンチマークでは、実際にお客様のアプリケーションを使ってサイズテストを行っています。ここでは、リンクしたコードと定数の合計サイズを、IAR Embedded WorkbenchのコードとRenesas CCのコード間で比較しています。

このアプリケーションテストから、IAR Embedded Workbenchで生成されたコードサイズは、Renesas CCRL比で28%減を達成しています。

Tools and options for RL78 code size benchmark

This is a code size test on real customer applications where the size of linked code + constants has been compared. The test was performed with the following tools and options:

CC-RL v1.10.00

ccrl -cpu=S3 -c -dbl_size=4 -dev=DR5F104PJ.DVF -g -Osize -Oalias=ansi -Osame_code

IAR EWRL78 v4.21

iccrl78.exe --core S3 --code_model near --data_model near --near_const_location rom0 -e --debug -Ohz --double=32 --no_scheduling

GCC for Renesas RL78 v4.9.2
rl78-elf-gcc -MMD -MP -Os -ffunction-sections -fdata-sections -g -mg14 -mrelax -mmul=g14 -c -x c

Kitchen oven display software kitchen_oven_display
Smallest Univalue Segment Assimilating Nucleus (SUSAN) susan
Telecommunication signal processing gsm_efr
Oven temperature controller temp_display
Bluetooth stack bt_stack
RTOS self-test application RTOS_test
Functions to descramble CSS encrypted DVD content. decrypt
Blowfish algorithm blowfish
Insert and extract bit fields bittest

 

無償の評価版をダウンロード

無償の評価版:IAR Embedded Workbench for Renesas RL78

評価版ライセンスは、完全に無償でその操作性をお試しいただけます。

ダウンロードをクリックすると、ライセンスを取得するためのユーザ登録が求められます。

 

14日の期間限定評価版ライセンスについては、以下の点にご注意ください。

  • 評価版ライセンスは14日間のみ使用可能です。
  • ランタイムライブラリにはソースコードが含まれません。(バイナリ提供)
  • MISRA C はサポートしていません。
  • テクニカルサポートは対象外です。
  • 製品開発を含む、いかなる商用開発にも使用出来ません。
ダウンロード

ユーザーガイド

Hardware debugging and RTOS support

Hardware debugging support

  • Renesas E2 Emulator
  • Renesas E1 Emulator
  • Renesas E2 Emulator Lite
  • Renesas EZ-Cube
  • Renesas IECUBE
  • Renesas E20
  • Renesas TK

RTOS support

  • Micrium μC/OS-II
  • OSEK Run Time Interface (ORTI)
  • embOS
  • Express Logic
  • FreeRTOS
  • CMX

Each RTOS plugin installs a number of new windows in C-SPY, most importantly the task or thread list windows where task-specific breakpoints can be specified and task-specific steps executed. Different inspector windows display the contents of the internal data structures of the RTOS such as timers, queues, semaphores, resources and mailboxes.

言語と規格

IAR C/C++ Compilerは、CおよびC++プログラム言語の各種方言や、組込みプログラミング用の様々な拡張機能に対応します(あらゆる実装に対応する言語規格をすべてサポートしているわけではありません)。厳格な規格コンプライアンスに対応するために拡張機能を禁止することも可能です。

一般的なデバッガやエミュレータのほとんどと互換性のある業界標準のデバッグおよびイメージフォーマットを幅広くサポートしています。これにはELF/DWARFなどが含まれます。

ISO/ANSI C/C++ へのコンプライアンス

IAR C/C++ Compilerは、次のようなCプログラム言語規格をフリースタンディングに実装しています。

  • INCITS/ISO/IEC 9899:2018、別名C18 (最新バージョンのみ)
  • IAR C/C++ CompilerはC++17のすべての機能に対応。C++ライブラリはC++14に対応、C++17追加機能のサポートなし。(最新バージョンのみ)

  • ISO/IEC 14882:2015、別名C++14

  • INCITS/ISO/IEC 9899:2012、別名C11

  • ANSI X3.159-1989、別名C89

IEEE 754規格

IAR Embedded Workbenchは浮動小数点演算のIEEE 754規格に対応しています。

MISRA C

MISRA Cは、MISRA (自動車産業ソフトウェア信頼性協会) が開発したCプログラム言語のためのソフトウェア開発規格で、SO規格のC言語で記述する組込みシステムでのコードの安全性、可搬性、信頼性を確保することを主な目的としています。

MISRA C規格の初版「自動車用ソフトウェアでC言語を利用するための手引き(Guidelines for the use of the C language in vehicle based software)」は、1998年に策定されました。2004年には第2版が作成され、規則番号の全面的な見直しなどの重要な変更が数多く行われました。さらに、拡張サポート付きのMISRA C:2012および安全でないコード構造を識別するためのMISRA C++:2008も規格に追加されました。

IAR Embedded Workbenchの特長であるアドオン製品 C-STATによって、MISRA C:2004、MISRA C++:2008、MISRA C:2012が策定した規則への準拠をチェックすることができます。

テスト検証

IARは、次のような市販のテストスイートを使って、IARのツールが規格に準拠していることを確認しています。

  • ISO/IEC Cへの準拠を確認するPlum Hall Validationテストスイート
  • C++への準拠を確認するPerennial EC++ Validation Suite

  • IARライブラリのC/C++規格への準拠およびC++規格に対するSTL実装を検証するDinkum C++ Proofer

上記の市販スイーツに加えて、いくつかの内製テストスイートを使用して、新機能の検証、リグレッションテスト、エラー修正に対する検証などを実施しています。

申し訳ございませんが、弊社サイトではInternet Explorerをサポートしていません。サイトをより快適にご利用いただくために、Chrome、Edge、Firefoxなどの最新ブラウザをお使いいただきますようお願いいたします。