Sensory 社は機械学習技術を使用した音声認識エンジンを提供しています。創業から25年にわたり音声認識技術に注力し全世界で数10億台以上のデバイスへの導入実績があります。このエンジンをRAマイコンに組込むことでネットワーク接続不要な音声認識ソリューションが実現できます。日本国内でのお問い合わせは株式会社グレープシステムまで。
Sensory の音声認識エンジンの1つである TrulyHandsfree は、音声によるボイストリガー・音声コマンド技術を提供します。最大30語の命令のキーワード・スポッティングやフレーズスポッティングが騒音下でも実行可能です。会話中のトリガーワードを認識して音声認識操作に移行することができ完全なハンズフリー操作が実現できます。
This demonstration will show voice recognition responses to a wake word phrase "Hey, Renesas" and some laundry-specific commands. This RA Ready Voice UI solution uses the Renesas RA6M5 MCU, DSP Concepts' two-microphone TalkTo™ audio front end and Sensory's embedded wake word and phrase recognition engines.