Detectors and sensors are surely one of the fastest-growing markets, being driven by the development of multiple applications within the Internet of Things. More and more detectors and sensors are used for monitoring purposes, especially in building automation systems, like access control system & security system or fire protection system. As a consequence, the detector kit is the perfect reference tool for your solution to the increasing demand for developing more intelligent sensors in a shorter time!
The Smoke Detector solution is an RL78 Quick Solution featuring the RL78/I1D. When the threshold is crossed and smoke is detected, an LED light will flash and an alarm will sound to alert users. Using the ultra-low power consumption RL78/I1D with built-in OPA, ADC, 12-bit IT, I/O, and other peripheral functions, reduce system costs and extends life of operation.
Every board has an adequate sensor depending on the measurement that needs to be done, on what needs to be detected:
All boards are featuring the new Renesas RL78/I1D microcontroller has the central element of the demonstrator board. Each detector or sensor application will benefit from the outstanding integration of the RL78/I1D MCU with his 4 channels of an operational amplifier, 2 channels of comparators in order to enhance processing capabilities.
The detector kit Detect-it! includes:
|
|
|
---|---|---|
分類 | タイトル | 日時 |
マニュアル-ハードウェア | PDF 2.72 MB | |
ガイド | PDF 294 KB | |
回路図 | ZIP 299 KB | |
パンフレット | PDF 1.70 MB | |
4 items
|