Over Past Decade, the Company has Sold More Than 100 Million PCIe Buffers in All

2014年12月18日

SAN JOSE, Calif., Dec. 18, 2015 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that it has shipped over 100 million PCIe buffers and over 3 million low-power PCIe Gen3 buffers, cementing its role as a key enabling and validation partner of leading x86 and ARM-based CPU and chipset suppliers.

IDT’s low-power PCIe Gen3 buffers apply IDT’s long-proven, patented, low-power HCSL (LP-HCSL) technology to address three major customer concerns. The buffers reduce operating costs (greatly reducing power consumption), save board space (eliminating up to 76 discrete termination resistors and also easing board routing), and support longer PCIe connection topologies (better signal integrity over long interconnects).

“These milestones underscore the fact that IDT gained its leadership in the PCIe timing market by delivering innovative solutions that address customer requirements,” said Dave Shepard, vice president and general manager of IDT’s Timing and RF Division. “We will continue to develop new PCIe technology that tackles the evolving challenges our customers face, hitting new milestones along the way.”

The 9ZXL family addresses PCIe Gen3 and QPI requirements commonly encountered in x86 data center applications. These devices are offered in 6, 8, 12, 15, and 19 output variants.

IDT’s 9DBU and 9DBV SOC-friendly PCIe Gen3 buffers offer the same PCIe performance as the 9ZXL devices in even smaller footprints and with even lower power consumption. While simultaneously supporting battery-powered operation, SOC-friendly PCIe Gen3 buffers maintain improved signal integrity over longer PCIe connection topologies. They are suitable for both x86 server and x86/ARM micro-server applications. The 9DBU and 9DBV families are offered with 2, 4, 5, 6, 7, 8, and 9 outputs and can be used for PCIe Gen3 applications in any system.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする