IDT's Low-latency, High-performance-per-watt RapidIO Switches Enable Prodrive and nCore to Use Texas Instrument’s RapidIO-compatible ARM+DSP Processors and Leapfrog Supercomputing Incumbents
SAN JOSE, Calif., June 17, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that the IDT CPS-1848 and CPS-1616 Gen 2 Serial RapidIO® switches provide the key system interconnect for the low-power BrownDwarf Supercomputer developed by nCore HPC and Prodrive. IDT's RapidIO switches offer 20 Gbps throughput per port with the lowest latency and the highest performance-per-watt compared to other interconnects, enabling nCore and Prodrive to use Texas Instruments’ (TI) RapidIO-equipped processors and leapfrog supercomputing incumbents.
The BrownDwarf supercomputer leverages TI's Keystone-II, which integrates multiple ARM® Cortex™-A15 MPCore™ processors, and TMS320C66x digital signal processors (DSPs) that feature embedded RapidIO Gen2 endpoints developed by IDT. BrownDwarf's three-shelf ATCA-based system delivers 70 teraflops of performance with 144 AMC-based nodes and 4032 processing cores. Taking into account the entire system power consumption, including processing, interconnect, and infrastructure, this equates to a very impressive 6.4 gigaflops per watt. In addition, the supercomputer is designed to easily scale using open standard RapidIO-based inter-cabinet switching, creating large multi-cabinet systems with up to 64K computing nodes.
nCore HPC and Prodrive selected IDT’s RapidIO switches for key benefits in throughput, latency, reliability and overall system power utilization that could not be achieved with Infiniband- or Ethernet-based approaches. IDT's RapidIO switches offer 20 Gbps of bandwidth per port, 100 ns cut through latency, 300 mW per 10 Gbps of data, up to 240 Gbps of non-blocking switch performance, and built-in reliable transmission. These performance, power, and reliability advantages are essential for supercomputer applications that leverage the power-efficient BrownDwarf platform.
“Our goal was to bring to market the most energy-efficient supercomputer,” said Ian Lintault, Managing Director of nCore. “We leveraged IDT’s RapidIO Gen 2 switches and TI’s RapidIO-equipped Keystone-II devices to create the highest-performance, lowest-power, non-NIC-based network fabric – an achievement that would not have been possible with InfiniBand® or Ethernet systems used by traditional supercomputing vendors. The BrownDwarf is expected to be in the top tier of the Green 500 world’s most energy-efficient supercomputers.”
“We have successfully deployed IDT’s RapidIO Gen2 switches for many customers across various embedded markets,” said Pieter Janssen, CEO at Prodrive. “Our past successes allowed us to quickly leverage the ATCA-based infrastructure for the BrownDwarf platform, going from concept to product launch in fewer than 6 months. RapidIO Gen2 is a key element of our computing solutions strategy and provides a graceful path to upgrade with RapidIO 10xN at 40 Gbps per port.”
“RapidIO is key to the multi-processor peer-to-peer processing needs that are emerging in both supercomputing and data center applications,” said Tom Sparkman, vice president and general manager of the Communications Division at IDT. “With the growth of processor-to-processor traffic in these applications, IDT’s RapidIO switches bring the critical attributes of embedded systems to offer improved system-level performance, throughput, latency, and energy efficiency.”
The IDT CPS-1848 and CPS-1616 belong to a broad portfolio of industry-leading RapidIO switch and bridge offerings. IDT provides a wide selection of port and lane count devices that allow customers to tailor their switch selection to the application. For more information about IDT’s RapidIO solutions, visit www.idt.com/go/SRIO.
nCore HPC’s BrownDwarf supercomputer will be available to qualified customers in the second half of 2013. Prodrive offers other form-factor developments or quick-turn customized solutions. Visit www.ncorehpc.com and www.prodrive.nl for more information. The BrownDwarf Supercomputer is being demonstrated at the International Supercomputing Conference (ISC) in Leipzig, Germany at booth 663 from June 17-20, 2013.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world, with direct purchase services through IDT Direct™. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.