The new product family leverages Wi-Fi 6/6E, BT/BLE 5.2 and Celeno’s novel Wi-Fi Doppler Radar to provide a connectivity and sensing solution for IoT end points, multimedia devices, and commercial applications
Celeno’s Doppler Radar can accurately locate people and distinguish complex types of movement such as falls, gestures and postures. It can even monitor motions that are difficult to detect like breathing
Ra’anana, Israel – Celeno Communications, a leading provider of smart, innovative Wi-Fi solutions, is launching the world’s first single chip solution for client devices combining Wi-Fi 6/6E, BT/BLE (Bluetooth® / Bluetooth® Low Energy) 5.2 and Celeno’s novel Wi-Fi Doppler Radar.
Celeno’s new CL6000 “Denali” product family provides a connectivity and sensing solution for devices such as consumer multimedia devices, IoT end points, home automation, industry automation, healthcare applications, etc. These new chips enable cloud connectivity with the latest Wi-Fi 6/6E standard, audio streaming and on-boarding use cases with BT and BLE 5.2 support, and sensing functions to enrich edge AI with valuable sensed data through its Doppler Radar function.
The product family supports both Wi-Fi 6 and Wi-Fi 6E standards with the latest advancements driving superior latency and robust connectivity, even in the most crowded Wi-Fi deployments. These include high bandwidth 160MHz channels, the new, recently approved 6-7GHz spectrum band, MU-OFDMA, MU-MIMO, Beamforming, 1024QAM, WPA3 encryption and Target Wake Time (TWT) for more efficient device power saving.
The CL6000 product family supports true simultaneous operation of Wi-Fi connectivity and Doppler Radar. The Doppler Radar is a Wi-Fi based, high-resolution sensing technology, that employs the Doppler effect and standard Wi-Fi packets.
The technology can track an object’s location or sense its presence or motion characteristics by using a single Wi-Fi device, without requiring the assistance of multiple devices or additional Wi-Fi clients. The solution leverages standard Wi-Fi and operates in the 5GHz and 6GHz bands, to “see” through walls without requiring line of sight and/or dependence on light conditions. In addition, the technology does not depend on any Wi-Fi clients, wearables of any kind and does not invade privacy.
Application Examples
The CL6020/10 can provide high speed Wi-Fi and BT/BLE connectivity for smart TVs and smart speakers to enable cloud connectivity and video share use cases.
The CL6025 can be selected to add sensing capabilities to multimedia devices, such as identifying human presence near the device or even for counting the number of TV viewers for driving various operational and monetization applications.
The CL6020/10 enables connectivity of IoT functions in sensors and cameras, to drive cloud-based security, safety and preemptive maintenance applications in smart buildings and factories.
Alternatively, by using the CL6025, the added radar function enables presence location and even posture recognition for supporting additional useful applications in buildings and homes, including human monitoring, elderly care and fall detection.
“We are excited to bring this disruptive solution to the Wi-Fi industry,” said Gilad Rozen, CEO and Founder of Celeno. “Celeno has been recognized for its innovative Wi-Fi solutions for home networking infrastructure applications. Our new CL6000 product family extends our product portfolio into the large Wi-Fi client markets, bringing together connectivity and sensing into smart home, IoT and multimedia devices.”
Main Product Variants
The product family consists of three main variants which offer optimized solutions for both high performance and price conscious applications:
- CL6025 – Supports 2T2R (2 Transmit and 2 Receive) MIMO configuration, tri-band selectable (2.4 / 5 / 6 GHz), BT/BLE 5.2 and Wi-Fi Doppler Radar – combined connectivity and sensing chip.
- CL6020 - Supports 2T2R (2 Transmit and 2 Receive) MIMO configuration, tri-band selectable (2.4 / 5 / 6 GHz), and BT/BLE 5.2 connectivity chip.
- CL6010 – Supports 1T1R (1 Transmit and 1 Receive) MIMO configuration, tri-band selectable (2.4 / 5 / 6 GHz) and BLE 5.2 connectivity chip.
The “Denali” CL6000 product family also shares the following main characteristics:
- Maximum traffic throughput of 2.4Gbps
- Internal RF Front End
- Host interfaces: PCIe-2 / USB3 / USB2 / UART
- Wafer Level Chip Scale Package (WLCSP)
The CL6000 product family will start sampling with customers in the first quarter of 2022.
About Celeno
Celeno offers advanced Wi-Fi chipsets and edge software to deliver smart, innovative Wi-Fi connectivity and Wi-Fi Doppler Imaging technology into the realm of high-performance home networks, smart buildings, enterprise, and industrial solutions. Celeno's field-proven chips and software technologies have been successfully integrated into numerous OEM Wi-Fi devices and have been deployed in tens of millions of homes around the world. Celeno is headquartered in Raanana, Israel, with global presence and offices. For more information, visit www.celeno.com
Media contact:
Amir Ben Artzi, Meirovitch PR, amir@meirovitch.com, Tel. +972-77-2129988
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.