Visit Booth# 121824 to Explore Renesas’ Industrial Network Solutions for Time-Sensitive Networking, Security, and Synchronized Distributed Motion at the Endpoint

2018年9月10日

MILPITAS, Calif. – Renesas Electronics Corporation, a premier supplier of advanced semiconductor solutions, will showcase its embedded innovation for the connected factory and Industrial IoT (IIoT) environments at the 2018 International Manufacturing Technology Show (IMTS), which takes place September 10-15 at McCormick Place in Chicago, Illinois.

During IMTS, Renesas will demonstrate several high-performance connected solutions featuring its RZ/N1 group of microprocessors (MPUs) and ICs for EtherCAT®, highlighting ways to increase efficiency, automation and security in industrial networking environments.

Technology Demonstrations

  • Renesas RZ/N1 Time Sensitive Networking (TSN)
    TSN is the next-generation IEEE 802.1 deterministic Ethernet standard for the IIoT that will unify the various fieldbuses into a single network infrastructure. This TSN demonstration highlights the RZ/N1 MPU as a TSN endpoint with time-synchronized communication that bridges the IT and OT domains and acts as a “gateway” that supports the TSN features of robustness, redundancy, and real-time operation required in the manufacturing (OT) domain, yet is compatible with IT bandwidth requirements.
  • Network Security for Endpoints
    Ethernet and IP protocols provide visibility to the outside world, enabling remote monitoring and time-based analytics, and improving overall efficiencies for connected factories, while also creating new security challenges. One solution: Design in security at the endpoint and network devices – typically resource-constrained embedded devices – rather than adding layers of IT-level network security. Renesas will demonstrate the design-in approach leveraging the RZ/N1 MPU with a network security framework that integrates an industrial-grade firewall and TLS, together with intrusion detection components to detect, report, and act on anomalous network traffic.
  • Distributed Motion with Renesas EC-1 EtherCAT ASSP
    One of the leading Industrial Ethernet protocols for automation applications, EtherCAT requires data cycle times as low as ≤ 100 µs, and low communication jitter. This demo highlights the high-performance capabilities of EtherCAT, with a distributed EtherCAT network and Renesas EtherCAT slave devices driving motors/discs spinning in tight synchronicity, while exploring the cost benefits of combining the EtherCAT slave controller and a real-time processor.
  • Real-time Industrial IoT Gateway
    Typical IIoT systems use IT-based gateways, which aggregate data from multiple systems and provide a cloud interface for trend analytics or remote monitoring but lack the granularity of real-time network data in the OT domain. The Renesas RZ/N1 enables an exchange of data between the two domains, partitioning between leading industrial networks for control, such as EtherCAT, Profinet, Ethernet/IP or even OPC UA, and cloud/on-premise platforms for deeper analytics. At IMTS, Renesas will highlight the RZ/N1 to demonstrate a secure, real-time, end-to-end gateway solution communicating as an OPC UA server that can be connected to any OPC UA client or to a cloud interface, extending the IT definition of the “edge” of the network down to the real-time domain of the machine itself.

For more information about Renesas, follow Renesas Electronics America at @RenesasAmerica on Twitter and https://www.facebook.com/RenesasElectronics.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) EtherCAT is a registered trademark and patented technology licensed from Beckhoff Automation GmbH of Germany. All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする