2015年4月27日

Düsseldorf, April 27, 2015 — Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, today announced the availability of its "Stream it!" kit, a complete evaluation platform for H.264 encoding and streaming in real-time. The new kit includes all the hardware, software components and demonstration programs manufacturers need to start development of cost-optimised video surveillance systems, video door phones, access control and intrusion detection systems.

Renesas' new "Stream it!" kit enables designers of advanced security and multimedia applications to develop scalable systems with the shortest time-to-market, reduced component count and optimised PCB footprint. The "Stream it!" kit comes pre-loaded with the H.264 Encode and Stream demonstration, but can also run two additional streaming demonstrations included in the kit. For developers of industrial sensor and home automation systems, the "Stream it!" kit can be used to log sensor status information, while sharing the collected data on a web server. For streaming applications targeting the consumer segment, internet radio MP3 files can be streamed to the "Stream it!" kit, decoded and played over headphones.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする