2012年9月11日

Dusseldorf, Germany, September 11, 2012 — Renesas Electronics Europe, a premier supplier of advanced semiconductor solutions, and Virtual Extension, an Israel-based provider of wireless mesh network solutions, today announced that they will be showing their new wireless digital addressable lighting interface (DALI) demo kit at the Strategies in Light Europe trade show (Munich, 18-20 September 2012). The new kit is based on Renesas’ RL78/I1A microcontroller (MCU), which combines in a single chip the LED control, power supply control, and communication functions required in lighting systems. These features are complemented by the innovative wireless mesh technology developed by Virtual Extension, enabling companies in the lighting industry to include intelligent controls in their products while reducing energy consumption. At Strategies in Light Europe, Renesas will be showing live demos of the new kit on stand A31, while Yariv Oren, CEO of Virtual Extension, will discuss wireless networks and DALI in his presentation on 19 September at 1:30pm during the Networks and Controls session.

DALI is an open standard that has seen significant success in Europe and continues to be adopted by the lighting industry, with over 50% of dimmable ballasts in the region supporting it already. Managing lighting in a commercial building using DALI is less expensive and more efficient than controlling it via a building automation system. It is also wireless-enabled, helping companies to overcome numerous obstacles for implementing DALI communications in their existing lighting infrastructure. As a result, the wireless feature of DALI facilitates an economical upgrade of any commercial building to provide a full-featured, digital lighting control system.

Against this backdrop, Renesas Electronics and its alliance partner Virtual Extension are releasing the new wireless DALI demonstration kit, which is based on the RL78/I1A lighting MCU. The new solution is built with a wireless gateway and 8 wireless nodes, all based on the Renesas RL78/I1A MCU which integrates the DALI function on a single chip. The gateway connects to the DALI Master controller to send and receive standard DALI commands. Each of the three LED channels in every wireless node has its own DALI address, which is used by the DALI Master for the remote and wireless control of each LED individually, or for broadcasting.

The system demonstrates wireless communications between DALI devices and particularly highlights the key benefits of Virtual Extension’s mesh topology used for this purpose. These include quick deployment, a high level of robustness, easy maintenance and low total cost of ownership (TCO). In addition, further unique advantages demonstrated by the Evaluation Kit include short and deterministic latency, scalability and low power consumption, all resulting from Virtual Extension’s VEmesh synchronized flooding technology. The RL78/I1A controls DALI communications, wireless network control, PFC control and driving multi-channel high power LEDs.

The wireless network uses Frequency Hopping Spread Spectrum (FHSS) and operates in the ISM/SRD sub-1Giga frequency band of 915MHz in US and 868MHz in Europe. Complying with European Telecommunications Standards Institute (ESTI) regulations on Adaptive Frequency Agility (AFA) and Listen Before Talk (LBT), the gateway and the nodes can make use of the maximum allowed transmission power. With 15 dBm output RF power, the range between any pair of wireless devices can reach 100m indoor and 500m outdoor. And this being a mesh network, where each network element serves also as a repeater, the network range can span to be tenfold or larger.

Following the demonstrations at Strategies in Light Europe, the evaluation kit will be released during Q4 and can be purchased from Virtual Extension.

(Remarks)
The new RL78 Family uses SuperFlash® technology licensed from Silicon Storage Technology, Inc. SuperFlash® is a registered trademark of Silicon Storage Technology, Inc., of the U.S.A. in the United States, Japan, and other countries. VEmesh is a trademark of Virtual Extension. All the other product and company names mentioned herein may be the trademarks or registered trademarks of their respective owners.

About Virtual Extension

Operating since 2000, Virtual Extension has pioneered the synchronized flooding technology based VEmesh networks for Smart Metering, Smart Lighting and Wireless Sensor Networks. The company’s OEM customers rate its products as having the best range, resiliency and simplicity of deployment. Virtual Extension provides a system that literally enables removing the wires from an existing sensor and replacing them with seamless connected wireless devices. Virtual Extension’s design wins power a diversity of applications, including pipeline security applications, agricultural, remote lighting, and industrial control and monitoring applications. For more information, please visit us at www.virtual-extension.com.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする