VDE certified software package is now available for the RX100 microcontroller’s family to quickly achieve safety compliance

2014年6月5日

Dusseldorf, June 05, 2014 — Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, today announced that it has received VDE certification for its IEC60335-compliant self-test software for the RX100 family of microcontrollers. This software, which is available for download free of charge from Renesas’ website, is fully compliant with IEC60730-1 regulations and has now been certified by VDE (the German Association for Electrical, Electronic & Information Technologies). The VDE Institute is recognized worldwide for its work on safety standards and approvals.

In addition to the on-chip hardware safety features, the self-test CPU software makes it easier for manufacturers of industrial, motor control and home appliances to meet IEC60730-1 (IEC60335) class B safety requirements. The safety standard requires software running on an MCU to be able to detect any safety critical failures according to specific fault models.

"This free software package designed for the RX100 MCU family offers high value to firmware developers involved in safety critical applications and appliances. For each RX family, including the RX600, RX200 and now the RX100, Renesas delivers VDE approved software to comply with the IEC60730/60335 safety standards,” said Vincent Mignard, Renesas' segment marketing manager for Home Appliances.

The RX100 MCU family integrates on-chip key advanced peripherals like the cyclic redundancy check engine (CRC) and a hardware clock monitoring function to detect erroneous clock frequencies. Finally, the RX100 offers the unique Data Operating Circuit (DOC) module, which reduces the RAM March X algorithms testing time and frees up the overall CPU load.

Renesas’ self-test software has been successfully certified for its periodic test routines for CPU registers and program counter tests, stack tests, RAM tests (using March X & C algorithms), Flash check (using cyclic redundancy check engines) and clock monitoring tests. These routines are easy to integrate in any existing software and can be called after reset and periodically during run-time. The software enables developers to easily design safety related software and to meet certification requirements quickly and with less effort. It can reduce development time and the test harness process by up to 3 months, and the cost of certification by 15%.

The complete software source codes in C and ASM for RX100, designed with the E² studio tool chain, is now available on the Renesas website at: http://www.renesas.en/support/downloads/download_results/C1000000-C9999999/mpumcu/rx/an_r01an2061ed_rx100_apl.html.

The package includes the official VDE certificate as well as the Application Note with the detailed timing of each routine and how to incorporate it into an existing project.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.

Remarks
All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする