Autonomous AI realized with low power consumption on R-Car V3H

Cortica

Cortica demonstrates at their booth and in-vehicle their unsupervised learning technology using the highly power-efficient CNN IP available in Renesas’ R-Car V3H SoC for premium front cameras, which is also equipped in the R-Car V3M for high-volume NCAP front cameras. Cortica demonstrates excellent detection of objects, whereas the implementation consumes very low power consumption on the scalable Renesas R-Car V3M and R-Car V3H SoCs.

Added on 2020-01-07

Cortica