The indoor sensor unit(s) for automatic home or building HVAC systems provide local data on each room or section via a Bluetooth® mesh to a master actuator. ​
This can be one or all of the following data:​

  • Indoor air quality (TVOC, eCO2 and IAQ according to the German Environment Agency, or UBA)​
  • Temperature and relative humidity (degrees, percentage)​
  • Light (lux)​
  • Barometric pressure (mbar)​
  • Motion detection​

In addition, a simple GUI can be implemented via capacitive touch or push button(s), and/or a low power LCD (i.e., eInk) to display local sensor values and enter data. A more sophisticated GUI may also be achieved via a master actuator, IP gateway or smartphone. A real-time clock (RTC) could easily be added to switch between different operation modes, depending on the day, time, holiday, etc. All RTCs could also be synchronized within the system.​

System Benefits​

  • The RX23W MCU enables Bluetooth 5 mesh communication​
  • The energy harvesting controller, the RE01 series, can be used for power supply. It combines the control of charging and discharging dedicated capacitors and/or rechargeable batteries of different sources with a powerful Arm® core MCU. These harvesters could be one of the following:​
    •   Solar cell (i.e., using the natural or artificial room lighting)​
    •   Thermal harvester (e.g., from a radiator or hot pipe)​
    •   Vibration harvester (e.g., from machines/motors)​
    •   RF harvester (i.e., taking away some of the near field energy from a close-by RF transmitter)​


 

Image
eu077-block-diagram

Related Products

Product Description Featured Document Ordering
       
Microcontroller      
RX23W 32-bit MCUs with Bluetooth® 5 for IoT endpoint devices, system control and wireless communication achieved on a single chip Datasheet Select Specific Device
       
Energy Harvesting Microcontroller      
RE01 Microcontroller based on Silicon on Thin Buried Oxide (SOTB™) process technology Datasheet Select Specific Device
       
Sensor      
ZSSC3224 High-End 24-Bit Sensor Signal Conditioner IC Datasheet Buy/Sample
HS3001 High-Performance Relative Humidity and Temperature Sensor Datasheet Buy/Sample
ISL29020 Low Power, High Sensitivity, Light-to-Digital Sensor With I2C Interface Datasheet Buy/Sample
ZMOD4410 Indoor Air Quality Sensor Platform Datasheet Buy/Sample