IDT's Multi-output, Low-power Timing Solution Features Less Than 0.7ps Phase Jitter and Superior Design Flexibility, Ideal for Cost-sensitive, Low-power Consumer and Low-jitter Communications Applications

March 11, 2014

SAN JOSE, Calif., March 11, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has extended its leadership in the timing market with the introduction of the VersaClock 5 family of programmable clock generators, featuring best-in-class jitter performance at half the power of competing devices. IDT’s multi-output timing solution consolidates system components with superior design flexibility, making it ideal for cost-sensitive, low-power consumer and low-jitter communications applications.

          The 5P49V5901 is an in-system programmable clock generator featuring four universal output pairs capable of producing independent frequencies up to 350 MHz in various output types. The highly-integrated device consolidates four differential or eight single-ended clock generators, and can store up to four different configuration settings, helping to minimize board space and bill-of-materials. With RMS phase jitter less than 0.7 picoseconds over the full 12 kHz to 20 MHz integration range, the new device meets the stringent jitter requirements of PCI Express® Gen 1/2/3, USB 3.0, and 1G/10G Ethernet. The high-performance clock generator operates at less than 100 mW core power (50 percent lower than competing devices), helping to ease system thermal constraints, reduce operating power expenses, and maximize battery life.

          “VersaClock 5 is the best-in-class, complete clock tree solution for cost-sensitive, low-power consumer and low-jitter communication timing applications,” said Christian Kermarrec, vice president and general manager of the Timing and Synchronization Division at IDT. “Architecting a clock tree can be a complex process that is often further complicated by the inflexibility of crystal oscillator frequencies and procurement requirements. VersaClock 5 solves these issues with inherent flexibility in frequency and output configuration, crystal consolidation, and world-class support tools.”

          The 5P49V5901’s four universal output pairs are each independently configurable as HCSL, LVPECL, LVDS, or dual LVCMOS outputs. The fractional output dividers driving each output pair are easily programmed via I2C while the device is operating in the system, lending itself to system tuning and margin testing. Unlimited in-system reprogramming is possible via I2C, whereas four banks of one-time programmable non-volatile memory provide flexibility for multi-project inventory consolidation or design changes in field or production units. Upon request, devices may be factory-programmed to the customer’s desired configuration.

          The high level of integration, flexibility, and performance enables system designers to address a multitude of applications, such as: consumer, networking, computing, industrial, communications, broadcast video, and medical. The new product is fully supported by IDT’s Timing Commander™ software platform, allowing engineers to configure and program their devices with an intuitive, time-saving graphical user interface (GUI). Pre-developed configuration files are available for the most common applications.

Pricing and Availability
          The IDT 5P49V5901 is stocked at all of IDT’s major distributors. The device is available in a 24-lead 4 x 4 mm VFQFPN package, and is priced at $4.50 each for volumes of 10,000 units. To download the Timing Commander software and related VersaClock 5 configuration files, visit www.idt.com/go/TimingCommander. For more information about IDT’s VersaClock 5 programmable clock generator, visit www.idt.com/go/VersaClock5.

About IDT Clock and Timing Solutions

          With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. IDT has also expanded its portfolio to include frequency control products, such as the XpressO® oscillators from Fox Electronics and an innovative line of MEMS oscillators that are rapidly replacing legacy quartz-based oscillators. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.