IDT’s Latest EyeBoost Retimer Improves PCIe Gen 3 Performance and Reliability by Restoring Signal Quality Across Long or Noisy Connections in Computing, Storage and Communication Applications

September 10, 2013

SAN JOSE, Calif., September 10, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the industry’s first 16-lane PCI Express® 3.0 signal-conditioning retimer. IDT’s new EyeBoost™ Retimer improves PCIe® performance and reliability by restoring signal quality across long or noisy connections in computing, storage, and communications applications. The device expands IDT’s industry-leading portfolio of packet switches and clock devices to offer a full PCIe 3.0 system interconnect solution.

          The IDT 89HT0832P is a 32-channel (16-lane) retimer capable of 8 Gbps-per-channel transfers, providing a total of 256 Gbps of communication bandwidth for data-intensive applications. The 89HT0832P is protocol-aware to support the PCIe 3.0-compliant equalization procedure for receiver and transmitter configuration, which eases system design-in complexity, and insures reliable low bit-error-rate (BER) operation with any PCI Express 3.0-compliant device, expansion card, or host bus adapter (HBA). The Retimer’s receivers include a high-performance continuous-time linear equalizer (CTLE) analog front-end followed by a five-tap decision feedback equalizer (DFE) and clock-data-recovery (CDR) circuit. This high-performance input with dynamic optimization can recover poor quality input signals, correct random and deterministic jitter, and boost transmit amplitude – enabling communication over long cables, long traces, or system backplanes.

          “IDT continues to lead the market in enterprise connectivity solutions by delivering the most advanced system interconnect products that customers are demanding,” said Sean Fan, vice president and general manager of the Interface and Connectivity Division at IDT. “Alternative solutions are limited to repeater-like devices that are not PCIe 3.0 standard-compliant, or expensive packet switch devices that consume significant and unnecessary power. Our latest EyeBoost PCIe Retimers offer a fully-compliant, high-performance solution for up to 16-lanes, and complement our 8- and 4-lane PCIe 3.0 Retimers to form the most complete portfolio in the industry.”

          The IDT 89HT0832P is compatible with 8-Gbps PCIe 3.0 and 5-Gbps PCIe 2.1, supporting the full PCIe 3.0 transmitter coefficient matrix, including boost and pre-shoot levels with high-swing options. It features automatic device calibration of key operating parameters, such as termination impedance and timing skews. This allows the device to self-adjust for manufacturing (wafer) or operating environment (voltage and temperature) variations to deliver optimum performance on a part-by-part basis. In addition, the device includes an internal pattern generator and scope for signal generation and capture. This enables system designers to produce signal eye diagrams and bit error contour charts for easy signal analysis, facilitating prototype system debug and remote field repair.

Pricing and Availability
          The IDT 89HT0832P is currently sampling to qualified customers and is available in 345-contact FCBGA packaging options of 13 x 20 mm body size with 0.8 mm ball pitch and 15.5 x 24 mm body size with 1.0 mm ball pitch. For more information about IDT’s signal integrity products, visit www.idt.com/go/SIP.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world, with direct purchase services through IDT Direct™. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on

Share this news on