IDT Expands Wireless Communications Portfolio with Glitch-Free DSA That Simplifies Software Interfaces, Improves Reliability, and Prevents Damage to Expensive Sub-assemblies

November 8, 2012

SAN JOSE, Calif., November 8, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced a new digital step attenuator (DSA) that reduces transient “glitches” during most significant bit (MSB) transitions by up to 95 percent in multi-standard 4G, 3G, and 2G cellular base station and industrial applications. IDT’s Glitch-Free™ DSA enables customers to simplify their software interface, improve reliability, and prevent damage to expensive sub-assemblies such as power amplifiers.

          The IDT F1950 and F1951 are digital step attenuators optimized for the demanding requirements of base transceiver station (BTS) receive, transmit, and digital pre-distortion (DPD) paths. IDT’s innovative Glitch-Free technology eliminates attenuation setting overshoot (glitches) from the transmit and receive paths of cellular communication systems, while at the same time reducing insertion loss and improving distortion performance. This significantly simplifies the hardware and software interfaces within the BTS, reducing cost and minimizing overhead. The extremely low IM3 distortion improves DPD path performance, enabling better transmitter spectral mask compliance and lower power consumption. The IDT F1950 (7-bit) and F1951 (6-bit) DSAs expand IDT’s comprehensive wireless communications portfolio, which includes RF mixers, variable gain amplifiers (VGAs), RapidIO® serial switching, industry-leading timing, data conversion and data compression products.

          “IDT’s new DSAs are another key building block of the communications signal chain that our customers are demanding,” said Tom Sparkman, vice president and general manager of the Communications Division at IDT. “Competing DSAs can glitch up to 10 dB during transitions of the MSB, while IDT’s Glitch-Free DSAs limit glitches to less than 0.5 dB – a significant performance advantage for our customers. In addition, our large attenuation range and high resolution gives customers the flexibility needed to service all the most popular wireless platforms. These latest products enhance an innovative portfolio of wireless communications solutions that is gaining strong traction in the marketplace.”

          The IDT F1950 and F1951 operate from 100 MHz to 4000 MHz, and can communicate via a parallel or serial interface. The devices are ideal for setting the power level in 4G long-term evolution (LTE), time-division duplexing (TDD), wideband code division multiple access (WCDMA), extended global system for mobile communications (EGSM) and other popular systems. The DSAs feature very low insertion loss (< 1.3 dB at 2 GHz) and are extremely accurate (< 0.2 dB over temperature), allowing for improved sensitivity and signal-to-noise ratio (SNR) in the receiver path.

Pricing and Availability
         The IDT F1950 and F1951 are in production and sampling to qualified customers. They are available in a 4 mm x 4 mm 24-pin QFN package. For more information about IDT’s RF solutions, visit www.idt.com/go/RF.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on

Share this news on