メインコンテンツに移動

ブログ

Solution for debugging and profiling multiple automotive devices

車載マルチデバイスのデバッグ/プロファイリングソリューション

協調動作が必要なマルチデバイス環境におけるソフトウェア開発の課題を解消するためのソリューションを紹介します。

Single MCU Solution for Safety-Related Applications Using TrustZone Blog

Single MCU Solution for Safety-Related Applications Using TrustZone

Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.

Power Up Your SPI Transfers

Power Up Your SPI Transfers

This blog looks at how we can automate a series of SPI transfers using the command sequencer implemented on many RA 32-bit MCU devices.

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution? Blog

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution?

Gigabit speed and its associated frequencies require sophisticated schematics and PCB design. Renesas’ Gigabit Industrial Ethernet SoM solution contains all of the needed mission-critical components.

Reducing Noise Issues in Microcontroller Systems Blog

Reducing Noise Issues in Microcontroller Systems - Part 4

In this blog, we look at some of the features implemented on RA microcontrollers that can help create reliable applications in the face of noise.

RH4Z2501: The New Robust IO-Link Compliant Transceiver

RH4Z2501: The New Robust IO-Link Compliant Transceiver

The IO-Link protocol (IEC 61131-9) is getting a lot of traction within the factory and process automation sector.

Renesas AI Panel Recap: Semiconductor Industry Is Pulling AI Across a Diversity of End Uses and Applications

半導体産業が多様な用途と応用でAIをリードする

半導体を活用してAIが普及していく期待と、半導体業界の中で設計やテストにAIが活用されている現状と展望を、キーマンらがパネルディスカッションした内容を紹介します。

 Accelerate Your Automotive Innovations with the R-Car S4 SoC Low Cost Evaluation Board Starter Kit Blog

Accelerate Your Automotive Innovations with the R-Car S4 SoC Low-Cost Evaluation Board Starter Kit

As the automotive industry is challenged to introduce software-defined vehicles (SDVs), it is crucial to have a low-cost and easy-to-use development environment for rapid software development.

Introducing the Handbook that Provides a Comprehensive Overview of RX140!

RX140のすべてが一目で分かるハンドブックのご紹介!

本ハンドブックでは、製品開発時に必要な資料やツール等を開発フェーズごとに纏めて一覧にしています。ユーザーは豊富なコンテンツの中から最適な情報をすぐに把握できます。