Overview

Description

Topics
New Release: The Embedded Target V6.06.00
The Embedded Target supports the device RA8T1.

We offer the above tool for co-simulation between the CS+/e² studio integrated development environment from Renesas interlinked with MATLAB® and Simulink® from the MathWorks, Inc. Among other things, this will support the validation of algorithms and model-based development by customers. For more information of this tool related to using evaluation version or purchasing commercial version, please refer to the release information.

Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.

Features

  • Generation of code for verifying algorithms from Simulink models
  • Automatic generation of Processor in the Loop Simulation (PILS) environments
  • Supported MCU families: RA, RX, RL78
  • What Customers Will be able to Do: Verify the functionality of code for target devices/Measure the performance of code for target devices
  • Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
  • Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
  • Learn More

Release Information

Latest Ver: V6.06.00.
Released: Jan 31, 2024

A license key is required to use the Embedded Target. Please check contents in below before using this tool.

For customer who consider commercial version of the Embedded Target

The Embedded Target is a tool that works with multiple software tools in tandem. Therefore, before purchasing commercial version license of this tool, we recommend that you check operating environments of the Embedded Target carefully and try the free evaluation version (limited 2 months usage) on your development environment first to check if it works properly.
This tool may not work properly under the following conditions.

  • MATLAB® versions are not supported by this product.
  • Specifications of Renesas MCU (such as small ROM/RAM size)
  • When a size of generated codes, which are affected size and complexity of the Simulink® model, is larger than ROM size of the MCU.
  • Inability to communicate due to network security settings, etc.

Again, please check operating environments of the Embedded Target carefully.

Embedded Target Evaluation Version Information

We will guide you through technical support.
Please refer to the following procedure.

  1. Access technical support on the Renesas Web site.
  2. Click on [LOG IN] and log in to the site with your ID which has been registered with My Renesas.
  3. Click on [SUBMIT A TICKET] in the upper right of the screen.
  4. Issue a new ticket by referring to the table and examples of entry which are shown to the right side.
    Title: Request a License Key for Evaluation version of the Embedded Target
    Inquiry Product Category: Microcontrollers & Microprocessors
    MCU Product Family: Renesas MCU (a device from the RA, RL78, or RX family) that is usable with Embedded Target
    Microcontrollers & Microprocessors: Technical Inquiry of MCU Tools
    Tool Name: Embedded Target for (the device you will be using) 
    Description: Describe the purpose for use and field of application for Embedded Target and your previous experience in using model-based development environments including MATLAB®.

Embedded Target Evaluation Version Information

Please check the "Software License Agreement" and "Licenses for Purchasing Commercial Version of the Embedded Target" in the detailed information, and contact your dealer, our sales representative, or our technical support.

Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.

Target Devices

Target Devices

Note

  • The Embedded Target may not work properly with certain ROM/RAM size of a device and/or size and complexity of a model.
    We recommend tying the evaluation edition on your development environment first to check if it works properly.
  • When using Embedded Target with an RA family device, an emulator and an actual device are required to perform PILS (Processor In the Loop Simulation). In addition, additional settings are required to match the FSP version and GCC version in use. For more information, refer to FAQ in below.
    FAQ: Project cannot be generated when using RA family in Embedded Target. (Embedded Target error code E300)

Downloads

Type Title Date
Upgrade - IDE Log in to Download ZIP 18.00 MB
Upgrade - Compiler Log in to Download ZIP 6.95 MB 日本語
Upgrade - IDE Log in to Download ZIP 753.29 MB 日本語
3 items

Documentation

Type Title Date
Flyer PDF 316 KB 日本語
Tool News - Release PDF 54 KB 日本語
Manual - Development Tools PDF 4.92 MB 日本語
Release Note PDF 289 KB 日本語
Tool News - Release PDF 44 KB 日本語
Tool News - Notification PDF 163 KB 日本語
Quick Start Guide PDF 4.27 MB
7 items

Design & Development

Reduce Time of Model-Based Development - Introduction of the Embedded Target

This video will introduce a useful software tool: Embedded Target. It can help developers reduce both testing time and costs in model-based development. Embedded Target can create an automatically configured model for the PILS environment. Next it generates a Renesas IDE project for PILS. Finally, model verification is performed by checking the execution time on an MCU or simulator.

Additional Details

Functionality

  • Generation of code for verifying algorithms from Simulink models
  • Automatic generation of Processor in the Loop Simulation (PILS) environments
  • Supported MCU families: RA, RL78, RX

What Customers Will be able to Do

  • Verify the functionality of code for target devices and
  • Measure the performance of code for target devices

Other Benefits to Customers

  • Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
  • Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
Image
em-concept-en

Software License Agreement

LicensesSoftware License Agreement
Node-Locked LicenseSoftware License Agreement (for Node Locked License) (PDF | English, 日本語)

Licenses for Purchasing Commercial Version of the Embedded Target

Give the part number from the list below to the distributor.

Embedded Target for RA family Node Locked License
PeriodNumber of LicensesPart Number
annual1RTCRA0000ET00WNJ
5RTCRA0000ET00WNJL5
10RTCRA0000ET00WNJLA
Embedded Target for RL78 family Node Locked License
PeriodNumber of LicensesPart Number
annual1RTCRL7800ET00WNJ
5RTCRL7800ET00WNJL5
10RTCRL7800ET00WNJLA
Embedded Target for RX family Node Locked License
PeriodNumber of LicensesPart Number
annual1RTCRX0000ET00WNJ
5RTCRX0000ET00WNJL5
10RTCRX0000ET00WNJLA

Learn More

For more information related with the Embedded Target commercial version or evaluation version, please contact a Renesas Electronics distributor, sales representative in your area or Technical Support on Renesas Web.