瑞萨电子一流的光/数字接近传感器具有低光灵敏度、卓越的接近范围性能、低功耗、易于使用的简单输出算法,以及一系列其他功能,包括智能中断、睡眠模式和飞行时间 (ToF) 信号处理。 我们的接近传感器和组合式光与接近传感器经过集成,可禁用电容式显示屏触控按钮,以防止手持式显示屏被意外按键激活。
Resolution (bits) |
Peak Spectral Sensitivity (nm) |
VS (Min) (V) |
VS (Max) (V) |
ICC |
界面 |
Counts/Lux (Max) (Counts) |
Dark ADC Code @ Ev=0Lux (Max) (Counts) |
Gain Selection |
启用 |
Address Selection Pins |
Lux Range (lux) |
Advanced Features |
Qualification Level |
Price (USD) | 1ku |
|
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
器件号 | |||||||||||||||
Time of Flight (ToF) Signal Processing IC | 2.7 | 3.3 | 1 µA (Shutdown), 55mA (Measuring) | I2C | 是 | Yes | 是 | Enables proximity detection and distance measurement | Standard | 5.44 |
Learn how to use the ISL29501-ST-EV1Z Sand Tiger Reference Design Kit to measure the distance and detect objects.
Hello, my name is Celine Baron. I am applications interim manager for optical products. I am going to show you now how to operate our Time of Flight ISL29501 Sand Tiger Reference Board. This is the evaluation kit you just received. In this evaluation kit you will find multiple components. The first one is a USB key that contains our software GUI to operate the board as well as the relevant technical documentation to perform your own evaluation.
You will also find, of course, our ISL29501 Sand Tiger board. If you open it, which is not necessary for the evaluation, you will be able to identify the optical components which are part of the system, a photo diode and an LED. The ISL29501 chip is located on the other side of the PCB. In the kit, you will find also a USB cable, that will allow you to connect the board to a PC for power and communication purposes. Last, you will find a black target. This black target will be used if you want to perform a manual calibration of the board.
I am going to show you now, how to quickly operate the board. First of all, install the GUI on your computer from the USB key and connect the board. Then you can open the tof.exe file that will start the GUI. And first you will read and accept our license. You will scroll down and click on 'Accept'. Then the board is ready to operate. You can confirm that the board is powered up, looking at the red LED that we have here. Let me demonstrate now how the part works.
First, I will load a profile clicking on 'File', 'Load Profile', and I select one of the two profiles available, then I just have to click on 'Start' and the board is completely operational. A first example of application is to point the board towards the target.
You can see two signals on the GUI, the magnitude and the distance in meters. Here I am measuring the distance between the board and the target. If now I introduce an object, my hand for instance, between the board and the target, you will see that the distance measure drops, because now I'm measuring the distance between the board and my hand. If my hand goes closer and closer to the board, the measure of distance obviously decreases.
More information on the GUI functionality is provided in the software manual. Thank you for watching.