Description

Uploads a file to a specified folder in a project.

CAll (METHOD = POST)

http://tool-cloud2.renesas.com/system/api/?key=[API_KEY]&module=object&action=updata&project=[PROJECT_NAME]&path =[FOLDER_PATH]&name=[OBJECT_NAME]
POST value:
upfile=>[FILE_DATA]

PROJECT_NAME: Specify PROJECT_NAME obtained as project information.

FOLDER_PATH: Specify the path to be uploaded. / indicates root.

OBJECT_NAME: Specify the file name to be uploaded.

Set the file data to upfile to be uploaded.

This will overwrite any existing file of the same name. Update history is not recorded.

Result


true or false