Cost Effective Solutions Offer Configurability, Flexibility and Scalability
2007年11月6日

 

SAN JOSE, Calif., November 6, 2007 – IDT® (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of essential mixed-signal semiconductor solutions that enrich the digital media experience, today announced a new family of devices - central packet switches (CPS) that address the interconnect needs of those embedded applications that utilize DSPs, FPGAs or processors.  The CPS solutions incorporate in-house third-generation IDT SERDES and serial RapidIO® core switch technology to provide customers with superior flexibility, scalability, performance, and power consumption at very competitive costs. These best-in-class switches provide significant system advantages in connecting virtually any digital media component to any other, in applications ranging from wireless infrastructure to enterprise storage, imaging applications, and beyond.
 
The CPS family enables combinations of performance, cost, and function previously impossible, by offering industry-leading flexibility, specifically  4x and 1x port options coupled with enhanced features for system bring-up and debug.   The CPS family of solutions includes three device configurations - with 16-port, 12-port, and 8-port options for 1x port counts. Moreover, the CPS family is pin-to-pin compatible with the IDT PPS Gen 2 family of devices, allowing customers the flexibility to upgrade their next-generation systems to the more powerful pre-processing solution with no impact on hardware or board design.
 
“The CPS devices are a great addition to our industry-leading portfolio of RapidIO solutions, which include our pre-processing switches and the 10G Serial Buffer. These newest enhanced solutions provide additional value-add benefit for our customers and to the markets they serve,” said Thomas Brenner, vice president and general manager for the IDT Flow Control Management Division. “Based on customer and industry feedback, we have learned that designers of the core technologies needed in digital media devices – they want to work with just one company that can reliably be their sole point of contact, from the physical elements of the device to every aspect of its operation, from board to system level. Whether its hardware or software, our customers want to be able to pick up a phone once, get a fast answer to their questions, and be done. We anticipate and address those needs by working with them when we’re developing solutions, and continue to partner with them from their design to post-production phases.”
 
Thomas continues, “Our customers recognize us as the industry best, not only on technical merit, but also on the partner-level support that we bundle with our solutions. This has helped us accelerate the acceptance of RapidIO as a standard, and resulted in a fast-growing range of major design wins across applications ranging from wireless base stations to high-end imaging.”
 
Leveraging the serial RapidIO®, JTAG and I2C interconnect standards, the IDT CPS family specifically addresses such markets as wireless and wireline, imaging, medical, military, IPTV, and other high-end communications markets and embedded applications. Following the IDT initiative to provide unparalleled performance in power smart configurations, the CPS family offers IDT customers a best-in-class solution through fastest possible time-to-market and smallest package size available for this class of products. Supporting software solutions provided for the CPS and PPS switch families include an IDT-developed calculator that allows customers to calculate power usage in various usage profiles. Customers can use this calculator to adjust device options to achieve maximum power savings. 
 
Based upon proven-IDT pre-processing technology, the CPS family includes an advanced feature set developed in conjunction with IDT customers to meet their specific interconnect needs. This feature set is built into the IDT solution to benefit customers when they are in the design phase, but also enables critical diagnostics during early stages of testing, and continues to be useful in the end-application. In addition, the CPS devices are configurable through any of the Serial RapidIO, JTAG, or I2C ports. The devices include a “loopback mode” which enables customers the added flexibility to work with the physical layer of the IDT device and quickly identify the source of any performance bottlenecks. Improving customer time-to-market, the CPS also incorporates useful diagnostics that provide customers with added security and faster time-to-market. These enhanced functions provide “kill” and “trace/mirror” capabilities that enable an added layer of security that is often critical in embedded applications.
 
About IDT Central Packet Switch Solutions
The central packet solutions are serial RapidIO-based switches whose functionality is central to routing packets for distribution among DSPs, processors FPGAs, other switches or any other serial RapidIO-based devices. They can also be used in serial RapidIO backplane switching. They support serial RapidIO packet switching (unicast, multicast and an optional broadcast) from any of their input ports to any of their output ports. The CPS-16 offers support for up to 16 ports of 1x or 4 ports of 4x (or combinations of 1x/4x), while the CPS-12 provides 12 ports 1x or 3 ports 4x (or combinations), and the CPS-8 provides 8 ports 1x or 1 port 4x with 4 ports 1x. Each switch offers full bandwidth support for its maximum port count and port speed options: the CPS-16 is 40 Gbps, the CPS-12 is 30 Gbps, and the CPS-8 is 20 Gbps. Each port can be configured for 3.125 Gbaud, 2.5 Gbaud, or 1.25 Gbaud, for long haul (backplane) or short haul (board) transmission profiles, with configurable drive strengths and pre-emphasis settings. The devices include IDT technical support available from product definition to application support.
 
Hardware/Software Development Kits Ease Evaluation and Design-In
The CPS solutions are supported by ATCA- and MicroTCA-compatible dedicated development platforms, designed in conjunction with Texas Instruments, together with a comprehensive range of software development tools, such as GUI, API, drivers and 3rd party tools. Each kit supports all other IDT pre-processing solutions and sRIO-enabled solutions such as the 10G Serial Buffer, and enables the designer to tune system and component configurations to meet system requirements. Moreover, to ensure that each system design is optimized for production and meets its time to market objectives, IDT provides customers with extensive collaborative support, including system modeling and signal integrity analyses, and schematic and layout review services.
 
Pricing and Availability
The CPS devices are available in a RoHS 324-ball BGA 19 mm x 19 mm, reducing package size in space-constrained applications. The CPS devices are currently sampling and are priced at $50 in 10,000 unit quantities for the CPS-16 (80KSW0002), $47.50 for the CPS-12 (80KSW0004) and $45 for the CPS-8 (80KSW0003). For additional product information on the IDT central packet switching solutions, visit www.IDT.com/go/CPS.
 
With the goal of continuously improving the digital media experience, IDT integrates its fundamental semiconductor heritage with essential innovation, developing and delivering low-power, mixed-signal solutions that solve customer problems.  Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com.
###
 
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章