ZL9117M Digital DC/DC PMBus 17A Module
Related Resources
Related Information
Related Videos
Video Transcript
Hi my name is Nattorn Pongratananukel I'm here at APEC 2012 demoing the ZL9117M power module, digital power module. So, the key benefit of this module is the high integration that we have combined with the digital power technology from Renesas. So in this demo I connect two evaluation boards together so that they can come up, stop start together. In the screen as I enable the path you see a waveform rise together at the same time. After this, I will artificially delay one channel after the other. So we can look at the GUI here.
So what I have done is delay the second channel 5ms from the first. Now we will look at the waveform after I enable it. We can see that the second channel now start up 5ms later than the first channel. And the last thing I want to show you with our power module is the snapshot feature. So, this snapshot feature is where you can ask the power module to save data as it encounters a fault condition.
According to the snapshot reading of the second channel we can see that the reading is normal. And the fault that I plan to create is to raise the input voltage from 5V to 6V and let the second module shutdown. From the eval board, we can see that the id line shutdown and from the scope, we can see the output of the second shutdown. While the first channel is still running. From the GUI, we will see that as I read this, it will report the last operating condition that second module has. If you want to learn more about the ZL9117M go to the Renesas website. Thank you very much.