Explain how to set up motor control evaluation kit "Motor RSSK"

Related Information

Use components like:

  • Featured List to link related documents (up to 3)
  • Text & HTML to list related links
  • Reference to link to a common text snippet

 

Related Videos



Video Transcript

Optional Transcript goes here if available. Read through the transcript text and link any appropriate keywords and products that have pages.

Example:

There are many 12V rails in industrial applications today that need a buck converter to step the voltage down to a lower voltage and deliver up to 14 amps. The ISL85009, ISL85012 and ISL85014 are pin compatible, very efficient and are able to deliver up to 14 amps.