electronica 2018 / SOTB™ Energy Harvesting / Battery-less ECG Heart Monitor

Demonstration of Battery-less ECG Heart Monitor. This demo shows sport bra with special material which allows to measure the heart rate or even full ECG without any battery. By using ultra low power SOTB™ Embedded Controller, system can be driven by harvested energy from solar cell only. It also shows a simple demo using two fingers.