Books on Renesas Technology
Published Books Covering Renesas Technology and Products
Note: a My Renesas ID is required to download the PDFs referenced on this page.
English
- Summary
- This introductory book for college sophomores to seniors covers the basic concepts of microprocessors and computers. Students will learn how hardware and software work together to create the computing foundation of today's electronics and embedded systems. Introductory theory is demonstrated with actual code examples highlighting the Renesas RX63N processor and evaluation board.
- Type
- Book
- Publisher
- Renesas Books
- Summary
- This advanced book for college seniors and graduate students delves deeper into modern interconnection concepts used in more sophisticated embedded systems. Theory of modern communications techniques are demonstrated with actual code examples highlighting the Renesas RX63N processor and evaluation board. Topics include Ethernet, CAN, USB, and advanced operating systems.
- Type
- Book
- Publisher
- Renesas Books
Miscellaneous
An Introduction to Computer Engineering using the Renesas Sakura Microcontroller Board
Mar 2018
- Summary
- This introductory book for high school students and college freshmen covers the basic concepts of the computer engineering field. Students will learn how to write software to control hardware devices. Introductory theory is demonstrated with actual code examples highlighting the Renesas RX63N-based Sakura Board. A fun application, building and controlling a line-following robot, demonstrates the field of embedded systems.
- Type
- Book
- Publisher
- Renesas Books
- Summary
- This book uses the Renesas RX62N family of microcontrollers to demonstrate concepts with hands-on examples complete with source code targeting the YRDKRX62N demonstration board. Geared for University education, this book is a wonderful reference and text for students and experienced engineers alike.
- Type
- Book
- Publisher
- Renesas Books
- Related Information
- Amazon.com
- Summary
- This book highlights how real-time kernels work, using Micriμm's μC/OS-III as a reference. The book consists of two parts: Part I describes real-time kernels in generic terms. Part II provides practical examples using Renesas' RX62N MCU.
- Type
- Book
- Publisher
- Micriμm
- Related Information
- Amazon.com
- Digi-Key
- Summary
- This two-part book puts the spotlight on how a TCP/IP stack works using Micriμm's μC/TCP-IP as a reference. Part I includes an overview of the basics of the Internet Protocol and walks through various aspects of μC/TCP-IP implementation and usage. Part II provides examples for the reader, using the Renesas YRDKRX62N Evaluation Board. The board features the Renesas RX62N, a high-performance 32-bit Flash MCU with FPU and DSP capability, and rich connectivity including Ethernet. Together with the Renesas e2 Studio, the evaluation board provides everything necessary to get you up and running quickly, as well as a fun and educational experience, resulting in a high-level of proficiency in a short time.
- Type
- Book
- Publisher
- Micriμm
- Related Information
- Amazon.com
- Summary
- Please click the following link for more details.
- Type
- Book
- Publisher
- Micriμm
- Related Information
- Micriμm
- Summary
- Please click the following link for more details.
- Type
- Book
- Publisher
- FreeRTOS
- Related Information
- FreeRTOS
- Summary
- An introduction to the design and optimization of embedded systems using the energy-efficient RL78 family of microcontrollers from Renesas Electronics Inc. The first portion focuses on design and covers microcontroller concepts, processor core, instruction set, interrupts, and peripherals for analog interfacing, communication, timing control, system robustness and acceleration, clocking and low-power modes. The second portion introduces concepts and methods for analyzing and optimizing a system's responsiveness, speed and energy use.
- Type
- Book
- Publisher
- Renesas Books
Miscellaneous
Embedded Systems Design, Analysis and Optimization using the Renesas RL78 Microcontroller
Mar 2018
- Summary
- This book explores concepts and methods for analyzing and optimizing a system's speed, responsiveness, energy and memory use. Program speed depends on creating an efficient program while helping the compiler generate fast code. Execution-time profiling finds the slow parts of the program quickly to guide optimization efforts. Program responsiveness to events depends on prioritization and preemption in the task scheduling approach. System energy efficiency depends on balancing a system's static and dynamic power consumption.
- Type
- Book
- Publisher
- Renesas Books
- Summary
- Embedded microcontrollers enable products with sophisticated control, precise timing, low unit cost, low development cost, and high design flexibility. This book shows how to design and optimize embedded systems using the energy-efficient RL78 family of microcontrollers from Renesas. The book is suitable for practicing engineers and both undergraduate and graduate classes on embedded systems.
- Type
- Book
- Related Information
- Amazon.com
Brazilian Portuguese
- Summary
- Um guia prático sobre microcontroladores de alto desempenho e daixo consumo de energia para sistemas embarcados
- Type
- Book
- Publisher
- Renesas Books