Statement on RoHS Recast

Renesas Electronics is strongly committed to compliance with all environmental laws, regulations and agreements that address our products as well as business activities. As such we have monitored requirements of RoHS (2011/65/EU) and (EU) 2015/863, and can conclude that our products are:

Renesas lead-free / RoHS compliant devices do not contain any of 9 substances known as hazardous substances (Cd, CrVI, Hg, PBB, PBDE, DEHP, BBP, DBP, DIBP), whereas lead (Pb) does not exceed 0.1% threshold by weight in homogenous materials, if not otherwise noted.

For detailed information, please contact your sales representative.

Title
Renesas' Statement on RoHS Recast
Renesas' Statement on RoHS Recast, April 2, 2018

Substances Restricted by the EU RoHS and its Maximum Concentration Value

Substances restricted by the EU RoHS Maximum concentration value (ppm)
Lead (Pb) 1,000
Mercury (Hg) 1,000
Cadmium (Cd) 100
Hexavalent chromium (Cr6+) 1,000
Polybrominated biphenyls (PBB) 1,000
Polybrominated diphenyl ethers (PBDE) 1,000
Bis(2-ethylhexyl) phthalate (DEHP) 1,000
Butyl benzyl phthalate (BBP) 1,000
Dibutyl phthalate (DBP) 1,000
Diisobutyl phthalate (DIBP) 1,000