Current consumption tuning solution

Renesas Electronics Corporation

Visualization of program and current change

As system current has become to be measured only by E2 emulator, repetition work of current reduction, which were previously done in a groping way, is made efficient and the work period is greatly shortened.
The following video shows current reduction debugging performed by the system using RL78.

Added on 2020-02-07

Visualization of program and current change - As system current has become to be measured only by E2 emulator, repetition work of current reduction, which were previously done in a groping way, is made efficient and the work period is greatly shortened. The following video shows current reduction debugging performed by the system using RL78.