Intrusion Prevention Solution in 400G Network Traffic
Renesas Electronics Corporation
This is a demo of the fastest 400Gbps class packet search that is applicable from data centers to backbone networks. By teaming up with Xilinx and employing a unique architecture from Renesas, this scalable reference design environment is able to shorten network equipment development time by up to 10 months.
The following video demonstrates the solution’s capability of monitoring illegal intrusions of up to 2 billion times per second.