Download (D6001884)

Issue Date : Nov.10.17

Category : Others

e-AI Translator V1.0.1



Description

The e-AI Translator is a tool that converts and imports the inference processing of neural network models which have been trained in an open-source deep-learning framework, Caffe or TensorFlow, into files of source code for the e² studio integrated development environment for MCUs and MPUs.
The e-AI Translator operates as a plug-in for the e² studio integrated development environment for Renesas MCUs and MPUs.


How to install

Need to install not only e-AI Translator but also license file.
Refer to the user’s manual for more details about installation.


Supported devices

RL78 Family, RX Family, RZ Family, and Renesas Synergy™ microcontrollers


Operating environment

Windows 7, Windows 8.1, Windows 10 (64-bit version only)

Download

Product Name File Name File Size Download Link
e-AI Translator V1.0.1 eAITranslatorV101.zip 775.01 KByte
License file for e-AI Translator V1.0.1 (Until May 31, 2019) license.txt 44 Byte