Channel Map Reporter


Example description

This example ads a couple of changes to the existing Proximity Reporter code in order to visualize the channel map usage during an active connection. Additionally some other parameters are shown over the serial interface like: peer Bluetooth address, connection parameters and disconnection including the disconnect reason.

The information is pushed out over the UART (P1_3, P2_3, 115200 baud, 8-bit, 1 stopbit, no parity, no flow control)

HW and SW configuration

  • Hardware configuration

    • This example runs on The DA14681 Bluetooth Smart SoC devices.
    • The Pro Development Kit (ProDK) or customer hardware is needed for this example.
    • The ProDK mainboard is combined with the daughter-board.
    • Connect the UART to a PC using the ProDK on-board FTDI serial-usb chip or a separate FTDI serial-usb cable.
  • Software configuration

    -This example requires:

    • Smartsnippets Studio 1.6.3.
    • SDK1.0.12
    • SEGGER’s J-Link tools should be downloaded and installed.
    • Terminal program @ 115200 baud, 8-bit, 1-stopbit, no parity, no flow-control.

How to run the example

Initial Setup

Connect your board (ProDK or customer board) to your computer.

  • Import the project into your workspace in the same directory as the pxp_reporter (subdirectory: demos)
  • Compile the project for the development Kit (Debug- or Release version).
  • Program it in the QSPI flash.

Use your favorite terminal program and connect it to the serial port (FTDI lower index port) with the following parameters

- baudrate: 115200
- data: 8 bits
- stop: 1 bit
- parity: None
- flow  control: none

After programming the device press the Reset button (K2). You should see the device entering a loop indicating:

Channel Map: 0000000000000000000000000000000000000000
Channel Map: 0000000000000000000000000000000000000000

###Connect to a master device

Take an Android- or Apple phone with a BLE application (like ‘LightBlue’) and scan for Dialog PX Reporter:

screenshot1|width=20%


Connect to the ‘Dialog PX Reporter’

Once connected the output over the UART will show the initial connection interval (about 50 mS) and the channel map info:

Connected to 55:6d:07:90:b3:cf
Connection parameters: Conn.Int: min=50.00, max=50.00 [mS], Slave lat: 0, Sup.Timeout: 20000 [mS]
Channel Map: 1111111111111111111111111111111111111000

After a short while the connection interval will change to the value set in the peripheral (pxp-reporter):

Connection parameters updated: Conn.Int: min=100.00, max=100.00 [mS], Slave lat: 0, Sup.Timeout: 20000 [mS] 
Channel Map: 1111111111111111111111111111111111111000

A ‘1’ indicates that that particular channel is in use. A ‘0’ means not is use. (The last 3 are the advertising channels 37, 38 and 39 and they are never used in connection).
UART output can be logged using a terminal program (Teraterm..)

Known Limitations

  • There are No known limitations for this example. But you can check and refer to the following application note for known hardware limitations.
  • Dialog Software Forum link.
  • you can Refer also for the Troubleshooting section in the DA1585x Getting Started with the Development Kit UM-B-049.

License


Copyright (c) 2015-2018 Dialog Semiconductor. All rights reserved.

This software (“Software”) is owned by Dialog Semiconductor.

By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.

EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIE, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.