May 28, 2014

Dusseldorf, May 28, 2014 — Renesas Electronics Europe, a premier provider of advanced semiconductor solutions, is pleased to announce that it has awarded its partner, Express Logic, with the status of Platinum Alliance Partner in Europe.

The Renesas Alliance Partner Program, comprising more than 800 companies, provides online tools to increase the synergy between customers, third party partners and Renesas. It allows customers to quickly find qualified design consultants, programming houses, tool vendors and manufacturing companies, providing faster time to market and an extension of their own design and development resources and expertise.

Awarding the status of Platinum Alliance Partner to Express Logic recognises their extensive experience in providing benefit to Renesas customers with a fully integrated platform for embedded system development that enables developers to create, produce and deploy exciting new products easily and successfully, both in Europe and around the world.

Steve Norman, Core Marketing Manager at Renesas Electronics Europe, said, “We welcome Express Logic to the select group of companies with Renesas Platinum Alliance Partner status in Europe. Billions of ThreadX deployments, certification for safety-critical applications and a wide portfolio of stacks and libraries supporting our microcontroller families means our customers can be sure of true software value and genuine speed to market.”

John Carbone, VP of Marketing at Express Logic, said, “We are honoured and delighted to be awarded Platinum Alliance Partner status by Renesas Electronics Europe. Our mutual customers have long benefited from the combination of our high-quality software and the powerful Renesas processors that it supports. As a Platinum Partner, we look forward to bringing this proven combination to even more developers throughout Europe.”

About Express Logic

Headquartered in San Diego, CA, Express Logic offers the most advanced run-time solution for deeply embedded applications, including the popular ThreadX® RTOS, the high-performance NetX™ and NetX Duo(tm) TCP/IP stacks, the FileX® embedded FAT-compatible file system, the USBX™ Host/Device USB protocol stack, and the GUIX™ graphical user interface development toolkit. Most products from Express Logic include full source code and all have no run-time royalties. For more information about Express Logic solutions, please visit the Web site at www.expresslogic.com, call 1-858-613-6640, or e-mail inquiries to [email protected].

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.

Remarks
All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on