Reduce Development Time, Safety Certification Risk, and Produce Highly Reliable, Safe Systems with the RX Microcontroller

November 25, 2013

TOKYO, Japan, November 25, 2013 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the development of a functional safety software package for its 32-bit RX631 and RX63N microcontroller (MCU) Groups. The new solution provides diagnostic software for the industry-leading RX CPU core and its internal memory, and a detailed safety manual to significantly reduce development time for designs that need to conform to stringent safety directives for industrial equipment, such as safety controllers, programmable logic controllers, industrial motor drives and safety sensors.

With the demand to improve safety in the workplace and reduce operating costs, the industry has initiated the need to implement functional safety standards according to IEC61508 to design inherent safety for control systems and equipment.

To conform to functional safety, system manufacturers need to perform safety analysis not just at the system level, but also down to the device level. Safety analysis includes failure mode analysis, consideration of diagnostic methods, and assessment of its diagnostic coverage. Doing these tests and trying to get detailed test analysis from the device manufacturer is a significant burden.

Renesas' safety solution for the RX631 and RX63N Group of MCUs has removed this burden by providing a self-test diagnostic software library and a complete safety manual.

Key features of the new functional safety solution:

(1) Safety manual

For the functional safety qualification, a comprehensive analysis targeting the IEC61508 functional safety standard is performed and the result is published in the safety manual. The safety manual includes the RX MCU's hardware safety mechanism, the diagnostic methods of software with its diagnostic coverage, and the safety parameter based on safety analysis for each function part of the MCU.

(2) Self-test diagnostic software library

A diagnostic software library for the CPU core, RAM and flash ROM. Since the diagnostic coverage of the CPU core has undergone comprehensive fault simulation tests (Note 1), the design solution makes it easy to show the basis of the coverage estimation and enables effective system integration.

(3) Compliant with the RX631/63N Group of MCUs

The new functional safety solution is compliant with Renesas' RX631 and RX63N MCUs. The RX631 and RX63N MCUs are high-performance, 32-bit MCUs that operate at 1.65 DMIPS/MHz, and include a floating point unit (FPU), hardware multipliers & MAC, flash operation without wait states, memory sizes up to 2MB of on-chip flash, and a rich set of peripherals such as multiple timers, high speed analog, Ethernet connectivity, and built-in safety-related functions. By using the new functional safety solution, system manufacturers can easily apply functional safety to their systems using the RX631 and RX63N MCUs. Renesas is also planning to expand this safety solution to the company's other RX family MCUs.

Exhibition at SPS IPC Drives

Renesas' functional safety solution for the RX631 and RX63N Group of MCUs will be showcased at SPS IPC Drives to be held in Nuremberg, Germany from November 26 to 28, 2013.

Availability

Renesas' new Functional Safety Solution will be sold under a software license model, and will be available in February 2014. (Availability is subject to change without notice.)

(Note 1) Fault simulation test:
A test to confirm diagnostic coverage of self-test software on the fault simulator.

(Remarks)
All other registered trademarks or trademarks are the property of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on