概览

简介

A Note to Users of the Peripheral Driver Generator
From now on, we do not intend to add or modify the support for devices by the Peripheral Driver Generator. We will be expanding support for devices by the Smart Configurator, particularly in the case of new devices.
Accordingly, although we will continue to support users of the Peripheral Driver Generator, we request that you consider the Smart Configurator.
Smart Configurator

The Peripheral Driver Generator is a utility that assists a product developer in creating various built-in peripheral I/O drivers of a microcomputer and the routines (functions) to initialize those drivers by eliminating the developer having to do manual coding. All of the necessary source codes are prepared by the Peripheral Driver Generator according to user settings, so that the development time and development cost can be greatly reduced.

The Peripheral Driver Generator is very simple to use, because all operations are performed through a user-friendly GUI. The status of peripheral I/O mode can be checked quickly and easily.

Also, a pin conflict between peripheral functions can be verified (V.2 only).

The Peripheral Driver Generator is a tool that you can install and use free of charge. Its operation is not guaranteed, although we have carefully evaluated the generated code. The user assumes all responsibility related to installing and using this tool.

Note CS+ (supports only Peripheral Driver Generator V.2), e² studio V3.0.0.22 and later (supports only Peripheral Driver Generator V.2), or High-performance Embedded Workshop.

特性

  • Elaborate Settings of Peripheral I/Os Accomplished Easily without the Need for Manual Coding
  • Ability to Avoid Incorrect or Forgotten Settings Related to Differing MCU Specifications
  • Advanced Setting Method Using Popup Window (V.2 Only)
  • Pin Window for Identifying Pin Conflicts (V.2 Only)
  • Displaying Pin Layout (V.2 Only)
    • MCUs involved: RX210, RX630, RX63N, RX631, RX63T
  • Learn More

发布信息

Peripheral Driver Generator V.2

Latest Ver.: V.2.09

Released: May 16, 2014

Details of upgrade (See Tool News)

Operating Environment

目标设备

下载

类型 文档标题 日期
软件和工具 - 其他 登录后下载 ZIP 162.85 MB 日文
软件和工具 - 其他 登录后下载 EXE 27.21 MB 日文
2 items

文档

Additional Details

The Peripheral Driver Generator and the library included in it are not evaluated in combination with the real-time OS environment. When using them, combined with the real-time OS, customers should consider the following use conditions in advance and then please use those at their own discretion.

  1. The functions and the library generated by the Peripheral Driver Generator are not the reentrant.
  2. The Peripheral Driver Generator and the library included in it do not take into account interrupt processing in the real-time OS.

Peripheral I/O Drivers Supported by the Peripheral Driver Generator

[Peripheral Driver Generator V.2]

MCU (Group) Peripheral I/Os for which drivers can be created and setup by the Peripheral Driver Generator
RX220 Clock, communication function (SCI, I2C, SPI), timers (MTU2, POE2, TMR, CMT, RTC, IWDT), buses, I/O, Interrupt control unit (ICU), A/D (12-bit), DMA (DMAC, DTC), CRC, LVD, Low power consumption, MPC, Clock frequency accuracy measurement circuit (CAC), Event link controller(ELC), Data operation circuit(DOC), Comparator (CMPA)
RX210 Clock, communication function (SCI, I2C, SPI), timers (MTU2, POE2, TMR, CMT, RTC, WDT, IWDT, TPU), buses, I/O, Interrupt control unit (ICU), A/D (12-bit, Temperature sensor), D/A, DMA (DMAC, DTC), CRC, LVD, Low power consumption, MPC, Clock frequency accuracy measurement circuit (CAC), Event link controller(ELC), Data operation circuit(DOC), Comparator (CMPA,CMPB)
RX630 Clock, communication function (SCI, I2C, SPI, IEB), timers (MTU2, MCK, POE2, TPU, PPG, TMR, CMT, RTC, WDT, IWDT), buses, I/O, Interrupt control unit (ICU), A/D (12-bit, 10-bit, Temperature sensor), D/A, DMA (DMAC, DTC), CRC, LVD, Low power consumption, MPC
RX63T Clock, communication function (SCI, I2C, SPI), timers (MTU3, POE3, CMT, WDT, IWDT, GPT), buses, I/O, Interrupt control unit (ICU), A/D (10-bit, 12-bit), D/A, DMA (DMAC, DTC), CRC, LVD, Low power consumption, MPC, Clock frequency accuracy measurement circuit (CAC), Data operation circuit(DOC)
RX63N, RX631 Clock, communication function (SCI, I2C, SPI, IEB), timers (MTU2, MCK, POE2, TPU, PPG, TMR, CMT, RTC, WDT, IWDT), buses, I/O, Interrupt control unit (ICU), A/D (12-bit, 10-bit, Temperature sensor), D/A, DMA (DMAC, EXDMAC, DTC), CRC, LVD, Low power consumption, MPC
RX62G Clock, communication function (SCI, I2C, SPI, LIN), timers (MTU3, POE3, CMT, WDT, IWDT, GPT), buses, I/O, Interrupt control unit (ICU), A/D (12-bit, 10-bit), DMA (DTC), CRC, LVD, Low power consumption
RX62T Clock, communication function (SCI, I2C, SPI, LIN), timers (MTU3, POE3, CMT, WDT, IWDT, GPT), buses, I/O, Interrupt control unit (ICU), A/D (12-bit, 10-bit), DMA (DTC), CRC, LVD, Low power consumption
RX62N Clock, communication function (SCI, I2C, SPI), timers (TMR, CMT, MTU2 (Note1), WDT, IWDT, POE2, PPG, RTC), buses, I/O, Interrupt control unit (ICU), A/D (10-bit, 12-bit), D/A, DMA (DMAC, EXDMAC, DTC), CRC, LVD, Low power consumption
RX610 Clock, communication function (SCI, I2C), timers (TMR, TPU, CMT), I/O, Interrupt control unit (ICU), A/D, DMAC (* Supports only little endian)

Note

  1. Except for complementary PWM mode and reset synchronous PWM mode

[Peripheral Driver Generator V.1]

MCU (Group) Peripheral I/Os for which drivers can be created and setup by the Peripheral Driver Generator
SH7125 Serial, timer (MTU2), I/O (Includes PFC), INT (external interrupt), and A/D
M16C/62P Serial, timer, I/O, INT (external interrupt), and A/D
M16C/28, M16C/28B, M16C/29 Serial, timer, I/O, INT (external interrupt), and A/D
R8C/13, R8C/22, R8C/23, R8C/24, R8C/25, R8C/26, R8C/27, R8C/28, R8C/29, R8C/2A, R8C/2B, R8C/2C, R8C/2D Serial, timer, I/O, INT (external interrupt), and A/D
H8S/20103, H8S/20203, H8S/20223 Serial, timer, I/O (Includes PMC), INT (external interrupt), A/D, DTC, and ELC
H8/3687, H8/36077, H8/36049, H8/36109 Serial, timer, I/O, INT (external interrupt), and A/D

Target Devices

[Peripheral Driver Generator V.2]

Family Series Group Support information
RX RX200 RX210, RX220 Peripheral I/O Drivers Supported
RX600 RX610, RX62N, RX62G, RX62T, RX630, RX63N/RX631, RX63T

[Peripheral Driver Generator V.1]

Peripheral Driver Generator V.1 is NOT available for V.6.00 Release 00 or later of the C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]. Use it with an old version in V.5.

Family Series Group Support information
SuperH SH/Tiny SH7125 Peripheral I/O Drivers Supported
M16C M16C/60 M16C/62P
M16C/Tiny M16C/28, M16C/28B, M16C/29
R8C R8C/2x, R8C/1x R8C/22, R8C/23, R8C/24, R8C/25, R8C/26, R8C/27, R8C/28, R8C/29, R8C/2A, R8C/2B, R8C/2C, R8C/2D, R8C/13
H8S H8S/Tiny H8S/20103, H8S/20203, H8S/20223
H8 H8/300H Tiny H8/3687, H8/36077, H8/36049, H8/36109