类别: Communication
BACnet Stack广泛应用于HVAC,照明和门禁控制应用,符合ISO 16484-5楼宇自动化和控制系统数据通信协议, 是经认证的, 符合标准的数据层应用, 适用于IP,以太网和BACnet MS / TP通信。堆栈的功能范围适合根据B-SS,B-SA,B-ASC和B-AAC等配置文件开发BACnet服务器。
BACeye软件工具允许轻松配置,监控和访问Bacnet设备及其对象和属性。
下载Synergy SK-S7G2套件上的BACnet应用软件,以演示BACnet堆栈和BACeye工具功能。
Download the BACnet application software on the Synergy SK-S7G2 Kit for a demonstration of the BACnet Stack and BACeye tool functionality.
Current Public Release
Release Date:2016-10-12
MCUs Supported: S7G2
MD5: d3438728f5151c824510955f933dbf5f
First release.
See Installation BACnet SSP1.1.0