创建安全的产品需要一整套的安全解决方案。 瑞萨可以指导您完成安全互联应用的设计和实施,涉及基本的安全概念、密钥处理,到进一步的云连接等高级主题,最后到批量生产和安全固件更新等领域。
瑞萨MCU独特的功能
颇具价值的安全认证
可定制的解决方案
全球合作伙伴
瑞萨独特的实现安全设计的方法基于一个原则:安全性需要嵌入到 MCU内部,以提供不可分割的硬件信任根。
请参阅各产品家族的网页,了解每个MCU的具体功能:
安全认证有助于提高人们对瑞萨安全产品的信心。 对于受监管行业应用而言,这些通常是强制性的认证。 它们还可以用于最终产品认证。
瑞萨致力于提供解决方案和各类工具,在为工程师提供自由的创新和差异化能力的同时,仍能满足紧迫的开发计划。 开箱即用,或根据需要定制。 请参阅以下的“文档”和“下载”部分,了解相关解决方案以及更多内容!
安全密钥安装
防止克隆、IP 盗窃和基础架构泄露。
安全启动,安全固件更新
帮助部署的产品保持最新状态,同时抵御最新的安全威胁。
安全通信
保护包括互联网和云连接在内的数据和基础设施。
防篡改
禁止访问设备内存和敏感信息。
从专门化加密和安全产品设计,到安全生产烧录和设备管理,我们的合作伙伴生态系统将随时为您提供帮助。 请务必查看瑞萨合作伙伴的安全导向的产品和解决方案,以进一步减少开发工作量并加速产品上市。
Title | Type | Description | Company |
---|---|---|---|
Security Key Management Tool | Solution Toolkit | A command-line tool for encrypting the RA family SCE's Protected Mode, DLM keys, Synergy SCE, or the encryption required when using the RX / RE / RZ family TSIP. | Renesas |
Flexible Software Package (FSP) | Software Package | FSP is an enhanced software package designed to provide easy-to-use, scalable, high-quality software for embedded system designs using Renesas RA Family of Arm Microcontrollers. Note: FSP with e² studio Installer (Platform Installer) will install the e² studio tool, FSP packs, GCC toolchain and Segger J-Link drivers required to use this software. No additional installations are required. |
Renesas |
Trusted Secure IP Driver | Security / Crypto | Trusted Secure IP driver software: this software supports AES with 128- and 256-bit keys), AES-GCM, AES-CMAC, and random number generation. Safely executes AES key management, secure updating of firmware, and secure booting at high speeds. | Renesas |
e² studio | IDE and Coding Tool | Eclipse-based Renesas integrated development environment (IDE). [Support MCU/MPU: RA, RE, RX, RL78, RH850, Renesas Synergy, RZ] (Note: You need to install compiler separately as an additional software) (Note: No separate e² studio installation required for RA FSP, this will be installed as part of the FSP with e² studio installer (Platform Installer) on GitHub.) |
Renesas |
Renesas Flash Programmer (Programming GUI) | Programmer (Unit/SW) | Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, Renesas Synergy, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78KR, 78K0] | Renesas |
|
|
|
---|---|---|
类型 | 文档标题 | 日期 |
样例程序 |
This application project discusses the considerations for securing Data at Rest in an embedded system and provides guidelines on how to use the Security MPU hardware feature of the RA Family MCUs to implement a secure Data at Rest solution.
ZIP
2.66 MB
Compiler:
ARMCC
IDE:
e2 studio
|
|
样例程序 |
[Software=RX Driver Package|V1.41],[Toolchains=CC-RX|V3.05.00;GNURX|8.03.00.202305;IAR Compiler for RX|v.4.20.01]
ZIP
393.84 MB
应用:
工业, 消费电子产品, 物联网(IoT)
Compiler:
CC-RX, GNURX, ICCRX
Function:
Security
IDE:
e2 studio, IAR EWRX
|
|
样例程序 |
MCUboot is a secure bootloader for 32-bit MCUs. It defines a common infrastructure for the bootloader, defines system flash layout on microcontroller systems, and provides a secure bootloader that enables easy software update.
ZIP
7.44 MB
Compiler:
GNU Arm Embedded
IDE:
e2 studio
|
|
样例程序 |
The application example provided in this package uses the Secure Crypto Engine (SCE) module based on RA6M3 to generate a device identity unique to each device which is securely stored in the internal flash using the Security Memory Protection Unit (MPU) and the Flash Access Window (FAW) hardware features of the MCU.
ZIP
9.74 MB
Compiler:
ARMCC
IDE:
e2 studio
|
|
样例程序 | ZIP 12.34 MB | |
样例程序 | ZIP 6.53 MB | |
样例程序 | ZIP 12.15 MB | |
样例程序 |
[Toolchains=GCC Arm Embedded|10.3.1.20210824] [Software=RA FSP] [Board=EK-RA2E1]
ZIP
18.39 MB
Compiler:
GNU Arm Embedded
IDE:
e2 studio
|
|
样例程序 |
The application example provided in this package uses the Secure Crypto Engine 9 (SCE9) module based on RA6M4 to generate a pair of ECC keys and uses a local CA to generate the device certificate based on the ECC public key.
ZIP
10.59 MB
|
|
样例程序 | ZIP 1.93 MB | |
样例程序 | ZIP 2.21 MB | |
样例程序 |
This application project is built with the integrated “Azure IoT SDK for Embedded C” package which allows
small embedded (IoT) devices like Renesas RA family of MCUs RA6M3, RA6M4, and RA6M5 to
communicate with Azure services.
ZIP
9.71 MB
IDE:
e2 studio
|
|
样例程序 |
ZIP
80.85 MB
应用:
工业, 消费电子产品
Compiler:
CC-RX
Function:
Application Example, OS
IDE:
e2 studio
|
|
样例程序 |
The application example provided in the package uses AWS IoT Core. The detailed steps in this
document show first-time AWS IoT Core users how to configure the AWS IoT Core platform to run this
application example.
ZIP
4.89 MB
IDE:
e2 studio
|
|
样例程序 | ZIP 2.91 MB Compiler: CC-RX IDE: e2 studio | |
15 items
|
Sixth in the RX security video series – Renesas walks through the process of encrypting the application program and performing a Secure Firmware Update using the Renesas Secure Flash Programmer so that the plain text of the application program to be updated is not exposed when updating the application program.
0:00:00 Opening
0:00:23 Recommended Viewing
0:00:53 Secure Factory Programming
0:02:10 Secure Firmware Update
0:06:45 For More Information
博客 | 2023年10月18日 | ||
博客 | 2023年5月23日 | ||
博客 | 2023年5月19日 | ||
博客 | 2022年10月18日 | ||
新闻 | 2022年5月19日 | ||
博客 | 2022年5月18日 | ||
博客 | 2021年5月20日 | ||
博客 | 2021年4月20日 | ||
博客 | 2021年2月13日 |