New Technology Allows for Greater Flexibility in Wireless Charging of Consumer Devices 

2012年10月30日

SAN JOSE AND SAN DIEGO, Calif., October 29, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) and Qualcomm Incorporated (NASDAQ: QCOM) today announced that the two companies have collaborated together to enable IDT’s development of an integrated circuit (IC) for consumer electronics devices based on Qualcomm’s WiPower™ Technology.  This IC will be designed to meet the requirements of Qualcomm’s new near-field magnetic resonance wireless power charging solution that is designed to provide spatial freedom for charging consumer electronics, such as mobile phones and other battery-powered/low-power direct-charge devices.

          “IDT’s leadership position in the wireless power industry has been proven by our award winning highly-integrated IDTP9030 transmitter and multi-mode IDTP9020 receiver chipset,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “We welcome the advancements that Qualcomm is making with WiPower technology, and plan to support its continued success by delivering the industry’s most innovative application-optimized solutions. IDT is excited to have been selected by Qualcomm to engage in this collaboration.”

          “We are pleased that IDT has collaborated with Qualcomm to design an integrated circuit based on our existing WiPower reference design,” said Steve Pazol, vice president of business development at Qualcomm. “We chose to work with IDT because they have proven their ability to develop compact, monolithic solutions. Unlike traditional consumer electronics wireless power solutions that bind the user to a charging mat, Qualcomm is looking to expand WiPower Technology into everyday surfaces, making it convenient for the user to top-off their portable devices throughout the day.“

          Developed by Qualcomm, WiPower technology uses resonant wireless energy transfer to elegantly reduce the amount of device chargers, unsightly power strips, and congested wall outlets to perform wireless charging, allowing for aesthetic charging pad designs that blend into a home, an office, and furniture. The power pads do not generally require a precise alignment of devices on the charging area or direct contact to charge a device, and can also charge multiple devices simultaneously.

          To learn more about Qualcomm’s WiPower wireless power technology and reference board, visit http://www.qualcomm.com/solutions/wireless-charging/wipower. For more information about IDT’s wireless power transmitter and receiver ICs, visit www.wirelesspowerbyidt.com.

About Qualcomm
Qualcomm Incorporated (NASDAQ: QCOM) is the world leader in 3G, 4G and next-generation wireless technologies. For more than 25 years, Qualcomm ideas and inventions have driven the evolution of digital communications, linking people everywhere more closely to information, entertainment and each other. For more information, visit Qualcomm’s websiteOnQ blogTwitter and Facebook pages.

About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.


IDT Contacts:
IDT Corporate Marketing
Graham Robertson, 408-284-2644
graham.robertson@idt.com

IDT Investor Relations
Mike Knapp, 408-284-6515
mike.knapp@idt.com


Qualcomm Contacts:
Tina Asmar, Corporate Communications
Phone:  1-858-845-5959
Email:  corpcomm@qualcomm.com

Warren Kneeshaw, Investor Relations
Phone:  1-858-658-4813
Email:  ir@qualcomm.com

###

Qualcomm is a trademark of Qualcomm Incorporated. WiPower is a trademark of Qualcomm Incorporated. Wi-Fi is a registered trademark of the Wi-Fi Alliance. All other trademarks are the sole property of their respective owners.


IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章