IDT Recognized for Innovative MEMS Oscillators, Wireless Power, and Data Converter Products

2013年11月14日

SAN JOSE, Calif., November 14, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has won three prestigious 2013 EDN China Innovation Awards. Spanning a wide spectrum of analog and digital technologies, IDT won ‘Best Product Award’ for its low-jitter MEMS oscillators, and two ‘Leading Product Awards’ for its dual-mode wireless power receiver and high-speed JESD204B-compliant data converters.

          “We’re honored to receive such prestigious awards for multiple products representing our analog and digital expertise,” said Jeff McCreary, president and CEO at IDT. “As an industry-leader of timing solutions, wireless power, and interface products, we strive to provide our customers with advanced performance and features that enable the development of next-generation consumer, enterprise computing, and communication infrastructure products. These awards are a testament to our success and validate our innovation and hard work.”

          IDT’s 4H-series MEMS Oscillators are the world’s first differential MEMS oscillators with only 100 femtosecond (fs) typical phase jitter performance and integrated frequency margining capability. The adaptable output frequency and extremely low phase jitter of IDT’s high-performance oscillators significantly reduce bit error rate (BER) in 10 gigabit Ethernet (10GbE) routers, switches, and other related networking equipment. IDT’s MEMS oscillator won the ‘Best Product Award’ in the Passive Components category.

          The IDTP9021  is the industry’s first dual-mode wireless power receiver IC that provides compatibility with both the Power Matters Alliance (PMA) Type 1 Interoperability Specification and Wireless Power Consortium (WPC) “Qi” standard. The dual-mode device bridges the technology gap between competing transmission standards, allowing customers to consolidate multi-chip configurations into a single-chip solution. The IDTP9021 is ideal for use in a myriad of mobile devices, including smart phones, tablets, MP3 players, digital cameras, MIDs, portable medical devices, remote controls, and other personal electronics. IDT’s wireless power receiver won a ‘Leading Product Award’ in the Power Devices and Modules category.

          The IDT DAC165xD is the industry’s first low-power dual 16-bit digital-to-analog converter (DAC) featuring the JESD204B high-speed serial interface. IDT’s high-speed DAC delivers best-in-class dynamic performance, eases system-level cooling requirements, and simplifies board routing in multi-carrier broadband wireless applications. IDT’s data converters won a ‘Leading Product Award’ in the Communication and Networking category.

          The winners of the 2013 EDN China Innovation Awards were announced on November 12, 2013 in Shanghai. For more information about IDT’s broad portfolio of analog and digital solutions, visit www.IDT.com.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章