IDT Extends Industry-Leading Portfolio of PCIe® Solutions with New Family of PCIe Gen 3 Switches, Offering up to 64 Lanes and 16 Ports

2012年3月15日

SAN JOSE, Calif., September 8, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has released the world’s highest performance family of Gen 3 PCI Express (PCIe) switches targeted at solid-state drive (SSD) storage arrays and cloud computing applications. The new family of switches builds upon IDT’s leadership in high-performance, scalable PCIe Gen 1 and Gen 2 switches, supporting a capacity up to 64 lanes and 16 ports with additional protocol enhancements for improved efficiency and reduced power consumption.


          IDT’s 89H64H16G3 is a 64-lane, 16-port Gen 3 PCIe switch, capable of up to 128 Gigabytes per second (GBps) switching capacity – the highest in the industry, making it the most scalable and highest-performance single-chip Gen 3 PCI Express solution on the market. The device conforms to the latest Gen3 PCIe specification providing 8Gbps link speed to enable the fastest PCIe connectivity possible for next generation enterprise server and storage systems. Added Gen 3 protocol enhancements improve overall efficiency and reduce power consumption, a critical factor for energy-conscious enterprise and cloud computing data centers. The device has been sampling to IDT’s lead customers for several months.

          “The future of Cloud Computing and PCIe SSDs rely on the advancements of PCI Express technology. As the leader in PCIe solutions, our customers rely on IDT to deliver the cutting-edge ICs needed to support their next generation designs,” said Kam Eshghi, Sr. Director of Marketing for the Enterprise Computing Division at IDT. “Our latest PCIe Gen 3 switches build upon our industry-leading portfolio of PCIe solutions and complement the industry’s first PCIe Gen 3 signal conditioning re-timers that IDT announced last November.”

          “IDT continues to be a strong contributor to the PCIe ecosystem,” said Jim Pappas, Director of Technology Initiatives, Intel Corporation (NASDAQ: INTC). “As the demand for enterprise storage and computing hardware grows, PCI Express will continue to be a critical system interconnect protocol. Intel is encouraged to see IDT's growing portfolio of PCIe Gen 3 switches and retimers.”

          The new family of IDT switches also includes clock isolation, offering the ability to operate with independent spread spectrum clocks (SSCs), as well as multicast for a significant gain in performance. Moreover, the switch incorporates a multi-root partitioning feature that allows designers to reduce system cost by replacing multiple PCIe switches with a single monolithic solution.

          To see this device in action, visit the Intel Developer Forum where IDT will be demonstrating Gen 3 PCI Express solutions. The event takes place from September 13-15 at the Moscone Center in San Francisco, California.

Pricing and Availability
The new switch family consists of the IDT 89H64H16G3, 89H48H12G3 and 89H32H8G3, which are 64/16, 48/12 and 32/8 port/lane counts, respectively. The devices are currently sampling to qualified customers and are available in 35x35mm, 27x27mm and 23x23mm BGA packages. For more information about IDT’s industry-leading portfolio of PCI Express switches, bridges, signal integrity, flash controller, and timing products, please visit www.idt.com/go/PCIeGen3.

 

About IDT          
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.