The IDTP9026’s Patented Technology Lets Customers Eliminate Many External Components, Helping Cut Costs While Reducing PCB Real Estate

2014年7月29日

SAN JOSE, Calif., July 16, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today announced the world’s smallest 2-watt wireless power receiver and battery charger, delivering leading technology in a compact package ideal for small form factors, including wearable applications. The IDTP9026 offers a high level of integration and lower external component count than competitive products, enabling designers to minimize board area and bill of materials. The device has a solution size requirement of less than 30 square millimeters, compared to 65 square millimeters for other available solutions. The chip is fully compliant with the Wireless Power Consortium’s (WPC-1.1) standards.

Part of IDT’s rapidly growing wireless power receiver product family, the IDTP9026 is a single-chip solution that utilizes patented technology to eliminate the need for many passive components traditionally required, helping OEMs cut costs while reducing overall application area without sacrificing performance.

“We strive to bring our customers innovative new products that help minimize expense and PCB real estate,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “The IDTP9026 helps designers reduce their design cycle-time with reduced costs and enhanced performance.”

The product’s I2C interface allows programming of the charging current, charging voltage, termination current and the thermal control loop for maximum flexibility and control.  Readings back from I2C include die and battery temperature, charging current and voltage, which can be used for custom control schemes or by the system’s application and user interface.

To complete the system, IDT recommends the IDTP9038 the industry’s first Qi-compliant single-chip wireless power transmitter supporting a 5V input. The two devices are fully compatible and are supported by IDT’s extensive design-in collateral and experience.

Product Availability and Pricing

IDTP9026 samples are currently available for select customers.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.