On‑Demand Webinar

We’re on a mission to make Wi‑Fi implementation simple and fast by adding a robust and comprehensive suite of AT‑Commands to our fantastic ultra‑low power Wi‑Fi family (DA16200 Wi‑Fi / DA16600 Wi‑Fi/BLE combo). Experience the industry leading ultra‑low power features of the DA16200/DA16600 family, simply, quickly, and effectively without the need to develop any complex software on the Wi‑Fi side.

During the webinar we will:

  1. Introduce the DA16200 ultra‑low power technology and show you how Wi‑Fi can work for battery powered applications
  2. Walk through the implementation using AT‑Commands (features/functions) – what it can do for your application
  3. Full end‑to‑end demo showing AT‑Commands on the Raspberry Pi Pico board (RP2040) as a host, hooked up to the DA16200 Wi‑Fi solution in an example application (Wi‑Fi connected Actuator – e.g. lock or motor) all with AWS IoT services connected to the DA16200

Presented by:

Ture Nielsen
Renesas Electronics
Product Marketing Manager

Ture Nielsen is the Product Marketing Manager of the IoT Wi‑Fi portfolio at Renesas Electronics with the mission to accelerate broad market adaptation to ultra‑low power Wi‑Fi products across IoT applications. Ture has a wealth of experience with more than 20 years in the wireless connectivity semiconductor industry, and more than 10 years of dedication to low‑power products.

Paolo Scarlata
Renesas Electronics
Principal Field Applications Engineer

Paolo Scarlata is an experienced Field Application Engineer with a demonstrated history of working in the semiconductors industry. He is skilled in Microcontrollers, Graphic Display Controllers, Memories, Power Line Communications, Embedded Software, IoT, Bluetooth, Wi‑Fi, Product Marketing, Semiconductors, Sales and Marketing Strategy. Paolo earned his Master's Degree in Electronic Engineering at the University of Palermo in Italy. His international career spans various positions at global players such as STMicroelectronics, Fujitsu, Spansion, Cypress, Dialog, and Renesas Electronics.

Register for instant access:

Not Me

By clicking submit you agree to the Renesas privacy policy.