On‑Demand Webinar

Ready to make your IoT development a piece of cake with the SmartBond™ DA14531 Bluetooth® Low Energy Module and CodeLess™ software?

The DA14531 SmartBond TINY Module is a Bluetooth LE solution that powers IoT devices through ease‑of‑use.

The DA14531 SmartBond TINY Module, based on the world’s smallest and lowest power Bluetooth 5.1 SoC, brings the DA14531 SoC advantages to an integrated module. It only requires a battery and a printed circuit board to build a complete Bluetooth application. The module is targeting broad market use and will be certified across regions worldwide, providing significant savings in development cost and time‑to‑market.

It comes with an integrated antenna and easy‑to‑use CodeLess software, making Bluetooth Low Energy development simpler than ever before.

This awesome combination takes mobile connectivity to applications previously out of reach, enabling the next billion IoT devices with SmartBond TINY at their core.

In this webinar, we will discuss:

  • The TINY™ Module: content, design, package, etc.
  • Worldwide certification
  • The development kit
  • CodeLess SW development and ready‑to‑use examples
  • Resources and support
  • How quick and easy it is to develop your new products with the DA14531 SmartBond TINY™ Module

Presented by:

Erik Peters
International Product Marketing Manager
Renesas Electronics

Erik is Product Marketing Manager for low power connectivity with a focus on Renesas' Bluetooth® LE portfolio. He joined Dialog Semiconductor (now Renesas) in 2017 as Regional Marketing Manager for Europe and is now responsible for proximity and automotive solutions.

Register for instant access:

Not Me

By clicking submit you agree to the Renesas privacy policy.