Silex Technology

Categories: Wireless

This project adds Wi-Fi connectivity using an external Silex ULPGN Wi-Fi module connected over a UART interface.

The project provides an example demonstration of the Renesas Synergy Platform connected to a Silex SX-ULPGN-EVK Wi-Fi evaluation kit. The demonstration covers the SX-ULPGN Wi-Fi Framework Application Programming Interface (API). It also includes the on-chip software stack and API and the Socket API for the SK-S7G2 development board. The SX-ULPGN is a single-band 2.4GHz 802.11n module based on the Qualcomm QCA4010 System-on-Chip (SoC).

SX-ULPGN-EVK Wi-Fi evaluation kit

new_releasesRelease Information

Copyright Disclaimer

Copyright © 2018 Silex. All Rights Reserved.

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

descriptionDocumentation

file_downloadDownloads

Synergy Download

SX-ULPGN Wi-Fi Drivers and PMOD

1.0

Current Public Release

Release Date:2018-03-08

MCUs Supported: S7G2, S3A7, S3A3, S5D9, S5D5, S5D3, S3A6, S3A1

MD5: 0e1bc009c3ddb4b65ee68ed717c7af67

Installation Instructions

  • wifi-addon-installer.exe – Installation executable to install the CMSIS pack file for the ULPGN drivers for Renesas Synergy
  • ulpgn_demo-20171218.zip – project file archivetcpserver.c – Additional optional file for use with the demo project, to set up a demonstration TCP server
  • udpserver.c – A UDP version of tcpserver.c

Detailed instructions are provided in the quick start guide with application note, driver code and demo is included.

Documentation & Support