This development assistance tool supports the development of embedded systems which use the camera functions of display controllers from Renesas. It supports MCUs of the RZ family.
Package | Component | |
---|---|---|
QE for Camera Latest Ver.: V1.1.1 Released: Apr 07, 2020 |
For RZ Family | QE for Camera[RZ] Latest Ver.: V1.1.1 Released: Apr 07, 2020 Operating Environment * QE for Display[RZ] is installed along with this product. (Previous product name: QE for Video Display Controller 5) |
|
|
|
---|---|---|
Type | Title | Date |
Application Note | PDF 266 KB | |
Tool News - Release | PDF 353 KB 日本語 | |
Tool News - Release | PDF 166 KB 日本語 | |
Release Note | PDF 149 KB 日本語 | |
Tool News - Release | PDF 111 KB 日本語 | |
Tool News - Release | PDF 142 KB 日本語 | |
6 items
|
The GUI allows the easy adjustment of the timing settings of a camera during testing. GUI displays with appropriate settings for various RZ/A target boards or custom boards for development are set up by selecting a target board or setting custom board configurations (Note1). The settings corresponding to those in the GUI display are created in a header file for direct incorporation in projects. If the value of a setting is not in accordance with the MCU spec., it is marked as being in error. This makes it easy for users to identify problems.
Note
Operation settings such as the image format and capture size of the camera module to be connected can be specified by sending a parameter file (csv file) from QE for Camera.
Even for a system that has no display device, such as a surveillance camera, interlinking with the in-memory image display function of the e² studio allows you to check images in the buffers for the VDC5.
A single button press writes the current settings to registers, so you can check the results for the actual camera and LCD panel. This tool also has a mode for automatically writing the changes to registers every time a setting is changed.
When you have finished the settings, the settings corresponding to those in the GUI display are created in a header file for direct incorporation in projects. QE for VDC5 can also operate in conjunction with the Supported Sample Programs.
Product Name | Sample Program |
---|---|
QE for Camera[RZ] | RZ/A1LU Software Package RZ/A2M Software Package |
RZ/A1H Group, RZ/A1M Group, RZ/A1LU Group, RZ/A1L Group, RZ/A1LC Group RZ/A1 Framework |
Product Name | Family | Series | Group |
---|---|---|---|
QE for Camera[RZ] | RZ | RZ/A | RZ/A1H, RZ/A1L, RZ/A1LC, RZ/A1LU, RZ/A1M, RZ/A2M |