The Art of Networking (Series 3): The Power of Virtualization Blog

The Art of Networking (Series 3): The Power of Virtualization

In this blog, we describe a proof of concept (POC) where we compare the benefit of having two virtual machines (VMs) sharing an integrated hardware switch against a software switch.

Merits of Using the Verified Linux Package in the RZ/G Board Support Package Blog

Merits of Using the Verified Linux Package in the RZ/G Board Support Package

This blog details the benefits of the Verified Linux Package which incorporates an industrial-grade Linux Civil Infrastructure Platform Super Long-term Support kernel in the RZ/G series’ Board Support Package.

Evaluation Environment for Dual Motor Control Using the Renesas RA Family RA6T1 Group Blog

Evaluation Environment for Dual Motor Control Using the Renesas RA Family RA6T1 Group

Using two of our already commercially available motor evaluation kits, users can control dual motors simultaneously by changing the motor control parameters on the simple provided GUI.

Realize OTA update using RX MCU with Bluetooth Low Energy (Bluetooth LE) wireless communication

Realize OTA Updates Using an RX MCU with Bluetooth Low Energy (Bluetooth LE) Wireless Communication

This blog introduces Renesas’ Over-the-Air (OTA) solution that uses Bluetooth Low Energy (LE) wireless technology to update the RX23W firmware from your smartphone.
Introducing the Wireless Evaluation Board from "Silex" that Can Easily be Used for Wireless and Total Power Evaluation of the BT5 Device Using the Renesas IDE Blog

Wireless and Total Power Evaluation of a BT5 Device Using Silex Evaluation Board and Renesas IDE

Easily get actual wireless and power evaluation even at a very early stage of the development using the Silex wireless evaluation board and Renesas’ IDE.

CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility Blog

CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility

The R9A06G037 CoolPhoenix 3 Powerline Modem (CPX3) has been re-certified to the PRIME Powerline standard Version 1.4 covering all security profiles as well as backward compatibility features.  

Renesas Quick-Connect, Now With Connectivity Options

Renesas Quick-Connect, Now With Connectivity Options

With the acquisition of Dialog Semiconductor by Renesas Electronics, Bluetooth and Wi-Fi connectivity options are now offered as part of the Renesas Quick-Connect IoT platform.

Things to Consider When Developing an ASIC Blog

Things to Consider When Developing an ASIC

Due to the non-homogenous nature of IIoT requirements, one size does not fit all in the IIoT. ASICs offer many advantages to a customer and working with the correct supplier is key to achieving these benefits.

100W Power Adaptor with Power Delivery and Wireless Charging Solution Blog

Carry Fewer Chargers with the 100W Power Adaptor with Power Delivery and Wireless Charging

The 100W Power Adaptor with Power Delivery and Wireless Charging Solution eliminates the need for multiple chargers by providing simultaneous use for wireless charging, USB-C with PD and two standard USB ports.

Smart Asset Tracking Label Blog

Smart Asset Tracking Label: The Future of Package Tracking

Our smart asset tracking label solution is a Bluetooth Low Energy, multi-sensor solution supporting data logging, real-time inventory and environmental data monitoring to prevent record and time-stamp inventory loss and damage.