The Ultra-Compact P9027 Offers Shorter Charging Times and Improved Thermal Performance

March 3, 2015

BARCELONA, Spain, March 3, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today introduced a new wireless power receiver that delivers faster charging in an ultra-compact form factor.  The P9027 magnetic induction receiver offers 80 percent peak system level efficiency and improved overall thermal performance. The high-efficiency architecture enables higher power transfer rates, translating into shorter charge times for portable devices such as smart phones and phablets.

Supporting the Wireless Power Consortium’s Qi standard, the P9027 is an 8 Watt receiver featuring an ultra compact solution size —approximately 37 square millimeters— and requiring six fewer capacitors than competitive products. The result is less board space and a lower bill of materials cost.

The device’s proprietary alignment guide optimizes inductive coupling with the transmitter to maximize coil-to-coil power efficiency. The 3 V to 7 V adjustable output voltage range is capable of driving a variety of downstream power management ICs, while proprietary foreign object detection (FOD) ensures safe operation in the presence of metal objects.

“As the technology inside our portable devices evolves, IDT continues to develop products to enhance the user experience while keeping product manufacturing costs low,” said Arman Naghavi, IDT’s vice president of Analog Power Technology. “The P9027’s thermal performance and size—teamed with its ability to lower BOM cost—make it ideal for the next generation of smart phones.”

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on