Renesas Introduces Bluetooth Low Energy Module for Ultra-Low Power IoT Applications

New RYZ012 Module Provides Multi-Standard Wireless Communication Supporting Bluetooth Low Energy 5 and IEEE802.15.4 Based Standards

04 Aug 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced sample shipment availability of the new RYZ012 Bluetooth® module targeting ultra-low power IoT applications. The RYZ012 is Renesas' first Bluetooth Low Energy 5 module. It integrates a 2.4 GHz RF transceiver supporting the IEEE802.15.4 multi-standard wireless protocol, Bluetooth Low Energy (LE), Bluetooth LE Mesh, and ZigBee. The RYZ012 features a power draw of only 0.4µA during deep sleep (without SRAM retention) allowing customers to extend battery life. The RYZ012 also includes a battery monitor to measure battery capacity and detect low power in battery-operated devices.

“The RYZ012 module complements our IoT connectivity solutions, featuring ultra-low power in a small form factor, designed to target a wide range of IoT, connected home, asset tracking, and cost-sensitive applications,” said Roger Wendelken, Senior Vice President, Head of MCU Business, IoT and Infrastructure Business Unit at Renesas. “The RYZ012 teams with Renesas’ sensor solutions to offer an end-to-end, device-to-cloud ecosystem.”

The RYZ012 module supports the 2.4 GHz IoT standards without the requirement for an external DSP. This reduces the number of external components required and the overall cost in system integration. The RYZ012 module includes a 32-bit microcontroller with an integrated 512kB flash memory and 64kB SRAM for application support. It comes in two versions: with and without an integrated antenna. This allows for implementation flexibility and the option for longer wireless range requirements.

The RYZ012 module will be certified for use in the U.S., Canada, EU, and Japan.

Availability

Samples of the RYZ012 module (both versions) are available now, with full product availability later this year. To order samples, please contact your local salesperson at www.renesas.com/support/contact.html.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) Bluetooth is a registered trademark of Bluetooth SIG, Inc. of the United States. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.