Intersil Announces Single-Chip Display Power and LED Driver for Smartphones

ISL98611 delivers higher power efficiency to extend battery life, and improve display image quality

Stock Price
Investor Relations

18 Aug 2014

MILPITAS, Calif., Aug. 18, 2014 (GLOBE NEWSWIRE) -- Intersil Corporation (Nasdaq:ISIL), a leading provider of innovative power management and precision analog solutions, today announced the ISL98611 display power and LED driver for smartphones. The ISL98611 is the first power management IC that integrates the display power and backlight LED driver functions in a single chip. It significantly improves efficiency of both functions to increase smartphone battery life by an hour or more.

 

A photo accompanying this release is available at http://www.globenewswire.com/newsroom/prs/?pkgid=27124

 

In addition to extending battery life, the ISL98611 also improves display brightness uniformity and color consistency. The highly integrated ISL98611 has a boost regulator, LDO and inverting charge pump for generating two output rails at +5V and -5V in a single device. It also includes a boost regulator with 3-channel current sinks for the LED backlight driver. This single-chip solution offers designers four key benefits:
 

  • Extended battery life: When used for web browsing and emails, a smartphone's backlight LEDs and display power consume the majority of its battery power. The ISL98611 backlight LED driver delivers seven percent higher efficiency (up to 93 percent) than competitive multi-chip solutions and generates +/-5V display power supplies with greater than 88 percent efficiency at 15mA load using a 2.5x2mm2 size inductor, compared to 85 percent efficiency of the nearest competitor.
  • Improved display uniformity: The ISL98611 provides excellent LED current matching at very low LED current: it achieves +/- 2.2 percent matching down to 1mA and +/- 2.8 percent at 50μA.
  • Improved display color consistency: The ISL98611 includes hybrid dimming to eliminate white LED color shift issues at low LED current, which occur with DC dimming.
  • Smallest footprint: The ISL98611's total display power plus backlight solution uses 24 percent less PCB area compared to the competition, while requiring only eight external components. This provides additional space to house the phone's battery.

 

"With each new product generation, smartphone designers are challenged to add more features, reduce size and extend battery life," said Andrew Cowell, senior vice president of Intersil's Mobile Power Products. "The ISL98611 delivers the integration, extended battery life and display image quality improvement our customers want in their next-generation smartphone designs."

 

Features and Specifications:

  • Powers two or three strings of backlight LEDs with up to 93 percent efficiency
  • Generates +/-5V display power supplies with 88 percent efficiency at 15mA load using a 2.5x2mm2 size inductor
  • Analog, PWM and hybrid dimming
  • +/-2.2 percent current matching down to 1mA and +/-2.8 percent at 50μA
  • 2.5V to 5V input voltage range
  • VP and VN output adjustable from +/4.5V up to +/-6V with 50mV steps
  • I2C, adjustable output voltage settings
  • 1uA shutdown supply current

 

Availability

The ISL98611 display power and LED driver is available now in a 2.33x2.61mm2, 30-ball WLCSP package. Pricing for the ISL98611 is $1.50 USD in 1k quantities. The ISL98611EVAL1Z evaluation board can be purchased for $100 USD each.

 

For more information on the ISL98611 display power and LED driver, please visit: www.intersil.com/products/ISL98611.

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.