IDT Announces World’s First Wireless Power Transmitter Solution that Supports Apple 7.5W and Android Fast-Charge Modes

Stock Price
Investor Relations

New transmitter supports Qi® Extended Power Profile and is compatible with the recent Apple® iOS 11.2 upgrade which allows users to enjoy the benefits of wireless fast charging

15 Dec 2017

SAN JOSE, Calif., December 15, 2017 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today announced the world’s first transmitter reference design for wireless charging of iPhone® 8 and iPhone X models with up to 7.5W of power, in addition to supporting WPC EPP and other Android-based fast charging modes. This new reference design is a compelling solution for designers and manufacturers of wireless charging pads, enabling them to create transmitters for Apple, Android and other devices that use the Qi wireless charging standard.

“Apple’s announcement in September to include Qi-based wireless charging in the latest iPhone models has dramatically increased user interest and with the recent release of the Apple iOS 11.2 upgrade, owners of these smartphones can now enjoy the benefits of fast wireless charging,” said Chris Stephens, general manager of IDT’s Mobile Power and Sensing Division. “IDT’s continued leadership in wireless power innovation is demonstrated in this converged solution which allows both Android and iOS smartphone fast wireless charging.”

At the heart of the reference design solution is the new IDT® P9242-G transmitter IC which provides for extremely accurate fixed frequency operation for EMI compatibility with EN303 417 and enhanced smartphone application co-existence. The reference kit supports the WPC Qi Baseline Power Profile (BPP) and Extended Power Profile (EPP) up to 15W with enhanced Foreign Object Detection (FOD) for a highly reliable and robust user experience. Additionally, the converged transmitter design supports all major fast wireless charging protocols.

The P9242-G-EVK reference kit has an input voltage range of 11V to 19V, supports USB or USB Type-C connectors and can be upgraded in the field through the system flash memory. The reference kit boasts extremely low quiescent power of less than 900mW.

IDT is sampling the product now and will release for broader availability in January, 2018. Visit idt.com/wireless power for more information including technical documentation.

 

© 2017 Integrated Device Technology, Inc. IDT and the IDT logo are registered trademarks or trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries in the United States and other jurisdictions. Qi is a registered trademark of Wireless Power Consortium. Apple and iPhone are registered trademarks of Apple, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners. IDT is not affiliated with, endorsed by, or associated with, Apple, Inc.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.