Skip to main content
Renesas Electronics Corporation

Overview

Description

Topics
e² studio supports the new device RX14T.

e² studio is an Eclipse-based integrated development environment (IDE) for Renesas MCUs. In addition to Eclipse’s own powerful code editor, e² studio offers a rich range of extended functions. e² studio covers all development processes, from the downloading of sample code to debugging.

Release Information

ArchitectureVer.Released
64-bit version2026-07Jul 24, 2026
32-bit version (Note1)V7.8.0Apr 20, 2020

Note

  1. Henceforth, only the 64-bit version of the e² studio is to have regular updates. Updates to the 32-bit version of the e² studio, on the other hand, will be limited to essential modifications.

Information on Usage

InstallationBuilding and Debugging
Generating Code
e² studio Integrated Development Environment User's Manual: Getting Started Guide RX, RL78, RH850 Family Rev.1.00 (PDF | English, 日本語)RX Smart Configurator User's Guide: e² studio (PDF | English, 日本語)

 

FAQ

Title
e² studio FAQs
Where can I find e² studio tutorial?
Project Migration from CS+ to e² studio

See all related FAQs

Target Devices

Downloads

Documentation

Design & Development

Explore

Videos & Training

Additional Details

e² studio

See the table below for features of the software and tools available for use with the e² studio on RX-family products. 
For an overview of the functions and features of the e² studio, refer to e² studio (the general page).

Code generation support and other useful functions for the RX family

Tool nameDescription
Smart ConfiguratorA GUI-based tool that provides support for downloading and importing middleware for code generation and configuring various settings
Smart ManualA function that allows you to find various information in a hardware manual, such as on registers, without opening the actual hardware manual
Smart BrowserA function that allows you to easily search and show the latest version of the hardware manual, technical updates, application notes, and tool news for the Renesas microcontroller you are using
Assistant for OptimizationA function that assists in optimizing the size of program code

 

Compilers for the RX Family

Supported CompilerInformation on Usage
Renesas 
C/C++ Compiler Package for RX Family [CC-RX] 
 
  • The version numbers which can be used with the e² studio:
    • For Windows: V2.00.01 and later versions
    • For Linux: V3.06.01 and later versions (Note1)
Open Source 
・GCC for Renesas RX
  • The GNU compilers can be installed through selection with the installer of the e² studio. This requires an Internet connection.
  • The GNU compilers can be installed free of charge by downloading from the GNU Web site (https://llvm-gcc-renesas.com). 
    Registration of these compilers with an e² studio which has already been installed is required.
IAR 
IAR C/C++ Compiler for Renesas RX
  • Debugging with the e² studio requires the building of load modules in the ELF/DWARF format.
  • IAR Systems provides plug-ins to handle projects for IAR compilers with Eclipse.
  • Contact IAR Systems K.K. for details:https://www.iar.com 

Note:

  1. CC-RX V3.06.01 supports Ubuntu version 20.04. Support for other versions of Ubuntu is under consideration for the next version.

 

Debugging tools for the RX Family

Note

  1. Installed in the e² studio as a standard item.
  2. Compatible with tools from IAR
  3. The usable functions of the E20 emulator for RX family MCUs other than those of the RX600 and RX700 series are the same as for the E1.
  4. Product from a Renesas partner

 

QE: Tools for Particular Applications for RX Family

Details: QE(Quick and Effective tool solution)

Simpler Development of IoT Devices Connectable with Cloud Service

The e² studio supports the development of software for IoT devices to be connectable with Amazon Web Services (AWS) or Microsoft Azure Cloud Computing Service. The e² studio offers the following powerful functions for FreeRTOS or Azure RTOS.

  • Quick building after downloading the latest version of FreeRTOS or Azure RTOS project directly from GitHub®
  • Assisting in configuring RTOS, all required drivers, network stacks (TCP/IP, Wi-Fi, and MQTT), and component libraries (Device Shadow, Azure RTOS NetX duo so on)(Note1)
  • Embedding additional middleware and drivers (such as for USB and file-system support) in IoT devices

Usage in detail (RX Family Amazon FreeRTOS download with e² studio Rev.1.00 (PDF | English, 日本語)) 

Image
The e² studio supports the development of software for IoT devices to be connectable with Amazon Web Services (AWS)

Note

  1. The settable components of RTOS are as follows: MQTT, Greengrass Discovery, Device Shadow, Azure RTOS NetX duo , Secure Sockets, and TCP/IP

Support

Support Communities

  1. ADC setting

    everyone, im new here in renesas, i want to setting ADC for RX 26T series, does have anyone here can show me the way to set up and how to use it in course code, i verry expecting your respond. thank you in advance. please help meee.

    Feb 26, 2025
  2. Rx140 Questions

    hello,  I bought the Rx140 kit and it's working.The debugger is using e2 lite, and the IC says R5F51406ADFN. Rx140 Cap Touch CPU Borad와 Self-Capacitance Button/Whee/Slider Electrode Board를 사용중입니다. I'd like to see Rawdata, Diffdata ...

    Jan 7, 2026
  3. I need pinout for 20 pin 0.05 inch header on E2 emulator

    ... the E2 emulator. I am using E1/E20/E2 Emulator, E2 Emulator Lite Additional Document for User’s Manual (Notes on Connection of RX Devices) as a reference to connect a RX63 device to the 14 pin connector. The E2 studio can't initialize the E2 emulator. I ...

    Oct 24, 2023
View All Results from Support Communities (61)

Knowledge Base

  1. Where Can I Find the e² studio Tutorials?

    ... at the e2 studio information web page for each device family. The manual shows basics of operation. It is recommended to read it through.e2 studio for RA Family: https://www.renesas.com/e2studio-rae2 studio for RZ Family: https://www.renesas.com/e2studio ...

    Dec 28, 2022
  2. I don’t know the ID code when I turn on E1 or E20. (E2, E2 Lite, E1, E20)

    ... in the ROM (flash memory for code storage) of the RX Family MCU. If you know which program (MOT or ABS file) you downloaded to the target MCU, you can obtain the ID code by reading the address of the program download with a simulator, etc.For more information on ...

    Mar 3, 2021
  3. How to See Toolchain Information of e² studio Project

    ... As shown in the examples below, toolchain type and version will be found in "Current Toolchain" box.Note that, if this box is empty, check the .cproject file description as mentioned later. Example of C/C++ Compiler Package for RX Family (CC-RX) :   Example of GCC Arm Embedded toolchain ...

    Jul 26, 2019
View All Results from Knowledge Base (14)