Skip to main content

PROFINET Device Software Start Guide

Jul 8, 2025

This video explains how to set up the sample program for the PROFINET Device. It covers running the PROFINET IRT DEVKIT on the RZ/N2L RSK and using the CODESYS PROFINET controller on a PC.

Chapter Titles

00:10 Introduction
00:37 Program Setup
02:35 Connection with PC
03:10 Download the program
04:03 Connecting to the controller and starting the demonstration

Related Resources