1. Home
    2. Technical Resources

Books

English

*A My Renesas ID is required for downloading the PDFs.

Cover Type Category Title Summary Publisher Related Information PDF
Book RX Embedded Systems: An Introduction using the Renesas RX63N Microcontroller This introductory book for college sophomores to seniors covers the basic concepts of microprocessors and computers. Students will learn how hardware and software work together to create the computing foundation of today's electronics and embedded systems. Introductory theory is demonstrated with actual code examples highlighting the Renesas RX63N processor and evaluation board. Topics include using modern development tools, software design, communications, firmware, and simple operating systems. Renesas Books  

Download*

Book RX Advanced Embedded Systems Concepts using the Renesas RX63N Microcontroller This advanced book for college seniors and graduate students delves deeper into modern interconnection concepts used in more sophisticated embedded systems. Theory of modern communications techniques are demonstrated with actual code examples highlighting the Renesas RX63N processor and evaluation board. Topics include Ethernet, CAN, USB, and advanced operating systems. Renesas Books  

Download*

Book RX An Introduction to Computer Engineering using the Renesas Sakura Microcontroller Board This introductory book for high school students and college freshmen covers the basic concepts of the computer engineering field. Students will learn how to write software to control hardware devices. Introductory theory is demonstrated with actual code examples highlighting the Renesas RX63N-based Sakura Board. A fun application, building and controlling a line-following robot, demonstrates the field of embedded systems. Renesas Books  

Download*

Book RX Embedded Systems, An Introduction Using the Renesas RX62N Microcontroller This book uses the Renesas RX62N family of microcontrollers to demonstrate concepts with hands-on examples complete with source code targeting the YRDKRX62N demonstration board. Geared for University education, this book is a wonderful reference and text for students and experienced engineers alike. Renesas Books Amazon.com

Download*

Book RX μC/OS-III: The Real-Time Kernel for the Renesas RX62N This book highlights how real-time kernels work, using Micriμm's μC/OS-III as a reference. The book consists of two parts: Part I describes real-time kernels in generic terms. Part II provides practical examples using Renesas' RX62N MCU. Micriμm Amazon.com Digi-Key

Download*

Book RX μC/TCP-IP: The Embedded Protocol Stack for the Renesas RX62N This two-part book puts the spotlight on how a TCP/IP stack works using Micriμm's μC/TCP-IP as a reference. Part I includes an overview of the basics of the Internet Protocol and walks through various aspects of μC/TCP-IP implementation and usage. Part II provides examples for the reader, using the Renesas YRDKRX62N Evaluation Board. The board features the Renesas RX62N, a high-performance 32-bit Flash MCU with FPU and DSP capability, and rich connectivity including Ethernet. Together with the Renesas e2 Studio, the evaluation board provides everything necessary to get you up and running quickly, as well as a fun and educational experience, resulting in a high-level of proficiency in a short time. Micriμm Amazon.com

Download*

Book RX μC/USB Device: Universal Serial Bus Device Stack for the Renesas RX63N Please click the following link for more details. Micriμm Link to external site  
Book RX FreeRTOS Tutorial Book, Renesas RX600 Edition Please click the following link for more details. FreeRTOS Link to external site  
Book RL78 Creating Fast, Responsive and Energy-Efficient Embedded Systems using the Renesas RL78 Microcontroller An introduction to the design and optimization of embedded systems using the energy-efficient RL78 family of microcontrollers from Renesas Electronics Inc. The first portion focuses on design and covers microcontroller concepts, processor core, instruction set, interrupts, and peripherals for analog interfacing, communication, timing control, system robustness and acceleration, clocking and low-power modes. The second portion introduces concepts and methods for analyzing and optimizing a system's responsiveness, speed and energy use. Renesas Books  

Download*

Book RL78 Embedded Systems Design, Analysis and Optimization using the Renesas RL78 Microcontroller This book explores concepts and methods for analyzing and optimizing a system's speed, responsiveness, energy and memory use. Program speed depends on creating an efficient program while helping the compiler generate fast code. Execution-time profiling finds the slow parts of the program quickly to guide optimization efforts. Program responsiveness to events depends on prioritization and preemption in the task scheduling approach. System energy efficiency depends on balancing a system's static and dynamic power consumption. Renesas Books  

Download*

Book RL78 Creating Fast, Responsive and Energy-Efficient Embedded Systems using the Renesas RL78 Microcontroller Embedded microcontrollers enable products with sophisticated control, precise timing, low unit cost, low development cost, and high design flexibility. This book shows how to design and optimize embedded systems using the energy-efficient RL78 family of microcontrollers from Renesas. The book is suitable for practicing engineers and both undergraduate and graduate classes on embedded systems. Renesas Books Amazon.com

Download*

Book SuperH μC/OS-III: The Real-Time Kernel for the Renesas SH7216 This two-part book puts the spotlight on how a real-time kernel works using Micriμm's μC/OS-III as a reference. Part I describes real-time kernels, while Part II provides practical examples using Renesas's SH7216 Ultra Fast MCU with FPU and Ethernet. Micriμm Amazon.com Digi-Key

Download*

Book SuperH μC/TCP-IP: The Embedded Protocol Stack for the Renesas SH7216 This two-part book puts the spotlight on how a TCP/IP stack works using Micriμm's μC/TCP-IP as a reference. Part I includes an overview of the basics of the Internet Protocol and walks through various aspects of μC/TCP-IP implementation and usage. Part II provide examples for the reader, using the Renesas YRDKSH7216 Evaluation Board. The board features the Renesas SH7216, a high-performance Superscalar Embedded Flash MCU with FPU, Ethernet and many other connectivity features. Together with the Renesas High-performance Embedded Workshop (HEW), the evaluation board provides everything necessary to get you up and running quickly, as well as a fun and educational experience, resulting in a high-level of proficiency in a short time. Micriμm Amazon.com

Download*

Cover Type Category Title Summary Publisher Related Information
Book RZ Interface 新定番の研究ARM×Linux 2013年11月号

In addition to explanation of the ARM core and Linux, this issue also contains an article about a remote temperature monitoring application experiment on Linux using a small board mounted with the RZ/A1L from Renesas' new product family. Comes with the "Handy Guide to Renesas Microcontrollers & Microprocessors 2013" as a supplement.

CQ Publishing Link to external site
Book RX GR-SAKURAではじめる電子工作 Even if you have no specialized knowledge, it is easy to get started with hobby electronics with Renesas' GR-SAKURA ("jee-ar sa-koo-ra") microcontroller board. This book presents and explains a variety of examples for people who are unfamiliar with microcontrollers or who have used Arduino but would like to try out another microcontroller board. Kohgaku-Sha Link to external site
Book RX RXマイコンのすべて 応用編 -RX62Nの「通信機能」を中心に、実際の使用例とプログラムが学べる- This book contains examples of actual use of communication functions (USB, TCP/IP, RSPI, and RIIC) built into the RX62N, and explains how to perform LCD direct drive, and so on. It can also be used as a convenient guide to the collection of sample code and application notes that can be obtained from the Renesas Electronics Web site. Dempa Shimbun Link to external site
Book RX RXマイコンのすべて 基礎編 -アーキテクチャからC言語プログラミングまで基本が学べる- The RX is Renesas' new CPU core. This book introduces the architecture of the new core and the basics of using it, such as how to create programs. It also describes how to increase program efficiency using the RX C/C++ compiler. A must-read for system developers, teachers, and researchers. Dempa Shimbun Link to external site
Book RX 動かしながら学ぶRXマイコン活用法 -RX62NのCPUボード付き!- This book takes an in-depth look at the new RX (Renesas eXtreme) microprocessor that was developed through the collected power of Renesas Electronics. It covers in detail the background that led to the birth of the RX MCU, its features and architecture, and how to use its development tools. Furthermore, the book comes with the RX62N mounted on a printed circuit board and a compiler and other development tools recorded on a CD-ROM, so that the reader can try out the capabilities of the RX right away. CQ Publishing

Link to external site

Link to external site

Magazine RX Interface 2011年5月号 RX62N基板付 RXマイコンではじめる組み込みプログラミング Embedded programming using the RX microcontroller CQ Publishing Link to external site
Magazine RX Interface 2011年6月号 万能RXマイコンにアレもコレも全部つなぐ ! Everything connects to the universal RX microcontroller! CQ Publishing Link to external site
Magazine RX Interface 2011年7月号 CPUの動作原理とアセンブラの基礎知識 Principles of operation of CPU and basic knowledge of assemblers CQ Publishing Link to external site
Magazine RX Interface 2011年8月号 USB機器開発トラの巻! ~実装の悩みを一挙解決 A bible to USB device development! Resolve board issues in a single stroke CQ Publishing Link to external site
Magazine RX Interface HDMI,DVI,DisplayPortディジタル映像信号の最前線 2011年9月号 技術解説 RX62Nマイコンを100%使いこなすために RXファミリ用C/C++コンパイラ活用技法~最適化編~ Technical article: In order to master the RX62N microcontroller 100% Techniques for using C/C++ compiler for RX Family: Optimization CQ Publishing Link to external site
Magazine RX Interface 組み込みの世界に接近するPC/ATアーキテクチャ 2011年10月号 技術解説 RX&SH-2Aで浮動小数点演算プログラムを記述する場合のRXマイコンのFPUを使いこなそう Technical article: Master the RX FPU for writing floating-point operation programs with RX & SH-2A CQ Publishing Link to external site
Magazine RX Interface 軽量Androidから組み込みミドルウェアまで 2011年11月号 技術解説 RX62Nマイコンを無線LANにお手軽につなごう! TCP/IPスタック内蔵無線LANモジュールの活用法 Technical article: Connect RX62N microcontroller to wireless LAN simply and conveniently! How to use the wireless LAN module with built-in TCP/IP stack CQ Publishing Link to external site
Magazine RX Interface 手を動かし実践する! MATLABプログラミング 2011年12月号 技術解説 RXマイコンで実現したUSB周辺機器をWindows上から制御するためのドライバ Windows Driver Foundation(WDF)によるデバイス ・ドライバ作成事例~KMDF編~ Technical article: Drivers for controlling USB peripheral devices from Windows using RX microcontroller: Windows Driver Foundation (WDF) devices - Example of driver creation: KMDF CQ Publishing Link to external site
Magazine RX Interface ユーザ・インターフェースの基本原則と実践開発 2012年1月号 技術解説 サイズ制限のないC コンパイラを使おう! RXマイコン対応KPIT Cummins GCC のインストールと使い方
Technical article: Use a C compiler without size restrictions! Installing and using KPIT Cummins GCC for RX microcontroller
CQ Publishing Link to external site
Magazine Smart Analog Interface 2012年4月号 内容: Smart Analogが変えるアナログ・フロント開発 第1回 Smart Analogとは何か Contents: Smart Analog changes analog front development. Part 1 - What is Smart Analog? CQ Publishing Link to external site
Magazine RX, Smart Analog Interface 2012年5月号 連載記事:第2回 Smart Analog ICをGIGSセンサで試してみよう Article series: Part 2 - Trying Smart Analog with a GIGS sensor. There is also an article about computer simulators of RX, SH-2, and others in the special features. CQ Publishing Link to external site
Magazine Smart Analog Interface 2012年6月号 連載記事:第3回 Smart Analogをマイコンと接続してみよう Article series: Part 3 - Connecting Smart Analog with a microcontroller CQ Publishing Link to external site
Magazine Smart Analog Interface 2012年7月号 連載記事:第4回 汎用OPアンプと基準電圧の利用 Article series: Part 4 - Using general operational amplifiers and reference voltage CQ Publishing Link to external site
Magazine Smart Analog Interface 2012年8月号 連載記事:第5回 A-Dコンバータの性能を100%引き出すプリアンプの作り方 Article series: Part 5 - Making a preamplifier that can draw out 100% performance from an A-D converter CQ Publishing Link to external site
Magazine Smart Analog Interface 2012年9月号 連載記事:第6回 「Smart Analog」と「PSoC」の設計コンセプト Article series: Part 6 - Design concept of Smart Analog and PSoC CQ Publishing Link to external site
Book V850 V850マイコン入門 This book is a introduction to basic knowledge about V850 microcontrollers and includes examples of applications created using V850 microcontroller boards. CQ Publishing Link to external site
Book SuperH SHマイコン活用記事全集 [1700頁収録CD-ROM付き] A compilation of articles about SH microcontrollers that appeared in Transistor Technology, Interface, and Design Wave Magazine from 2001-2010. CQ Publishing Link to external site
Book SuperH TECH Iシリーズ Vol.49 SH-2Aマイコン組み込み講座 An introduction to embedded microcontroller technology using the SH-2A core. Not simply an explanation; each chapter also contains practice programs (exercises) on controlling external I/O. Can be used together with the separately sold board (CQK-SH2A) to run programs on an actual device and perform debugging exercises. CQ Publishing Link to external site
Magazine SuperH Interface 2010年9月号 Continuing from the October 2010 issue of Interface, the technical article in this issue covers programming techniques for maximizing CPU performance. It describes how to use the option settings and optimization function of the compiler, and how to use the internal memory to improve performance. CQ Publishing Link to external site
Magazine SuperH Interface 2010年8月号 This issue highlights an example of a simple MP3 player created using the SH7262 board that was included with the June 2010 issue of Interface. It also contains a technical article that describes programming techniques for maximizing CPU performance, porting μC3/Compact real-time OS, and introduces an LCD expansion board that is compatible with the board that came with the June issue. CQ Publishing Link to external site
Magazine SuperH Interface 2010年7月号 In this issue, the use of display functions and peripheral functions such as USB of the SH7262 are explained in detail, as application examples of the SH7262 board that was included with the June 2010 issue of Interface. Sample programs for graphic display and touch panel applications using the SH7262 board are included. CQ Publishing Link to external site
Magazine SuperH Interface 2010年6月号 1. SH-2A Product Lineup and Functions of SH7262 explains the features of SH-2A products and the lineup, and gives an overview of the specifications of the SH7262. PDF (size: 237 KB) 2. How to Use the HEW Development Tool and How to Create Sample Programs explains how to install and use the development tool and how to create sample programs. PDF (size: 253 KB) 3. How to Use the Timer Controller and Interrupts explains the compare match timer and how it is used in the sample program. PDF (size: 226 KB) 4. The June 2010 issue of Interface comes with an SH7262 board. CQ Publishing Link to external site
Magazine SuperH Interface 2010年4月号 1. How to Use the SH-4A Processor with Built-in PCI Express Controller explains the initialization of the PCI Express built into the SH7786, the procedure for accessing memory, and so on. PDF (size: 239 KB) 2. Running Android on an SH7724 Board explains the procedure for running Android on a board mounted with the SH7724 (SH-MobileR2R). PDF (size: 281 KB) CQ Publishing Link to external site
Magazine SuperH Interface 2009年8月号 Implementing Graphics Display for Embedded Devices explains how to implement the display functions of the SH7764 with built-in high-function LCD control function. PDF (size: 131 KB) CQ Publishing Link to external site
Magazine SuperH Interface 2008年4月号 SH2A: Multi-Core and Software Support explains the CPU startup method of the dual-core SH2A-DUAL and support for OS and applications. PDF (size: 114 KB) CQ Publishing Link to external site
Book SuperH C言語によるSH-2マイコン プログラミング入門 This book uses the commercially available SH7145F microcontroller board to explain each peripheral function of an SH-2 microcontroller one by one, with many specific programming examples that the reader can experiment with. Recommended for people who wish to go to the next level of using SH-2 microcontrollers. Gijutsu-Hyohron Link to external site
Magazine SuperH Interface 2006年6月号 Introduction to Embedded Microcontrollers Using the SH-2 Board explains how to use the SH-2 (SH7144F) board that comes with this issue. CQ Publishing Link to external site
Magazine SuperH Interface 2005年2月号 The special feature Motor Types and Control presents an application example of single-shunt control of a brushless DC motor and the SH7046 motor control evaluation board. CQ Publishing Link to external site
Magazine SuperH Interface 2005年1月号 A series of articles on introductory design using the SH7047 were published starting from the January 2005 issue. CQ Publishing Link to external site
Book SuperH Design Wave Magazine 5月号 Examples of mechatronics control using the SH7727 appear in chapters 4 and 5. CQ Publishing Link to external site
Book SuperH 組み込みエンジニアのためのEmbedded UNIX Vol.3(絶版) Contains a special feature on creating a broadband router using SH-4. - Mounting of router function / secure protocol / VoIP using SH-4 board and Linux - Construction of Linux kernel, mounting of IPsec protocol, etc. CQ Publishing Link to external site
Book SuperH トランジスタ技術SPECIAL No.81 はじめてのSuperHプロセッサ入門(絶版) This book is perfect as a textbook for beginners to SH microprocessors. It explains everything from SH architecture to actual hardware and software development using the SH7045F, and programming the on-chip flash memory, in an easy-to-understand way. Please make use of it. CQ Publishing Link to external site
Magazine SuperH Interface 増刊 組み込みエンジニアのためのEmbedded UNIX Vol.2(絶版) This issue contains articles on embedded Linux system development using SH processors. CQ Publishing Link to external site
Book SuperH SuperHファミリのCプログラミング This book covers the knowledge required for programming the SuperH Family (both microcontrollers and microprocessors) in C. It presents effective ways of using FPU and DSP coprocessors, exception handling, and cache memory, and ways to increase development efficiency for software engineers. Ohmsha Link to external site
Book SuperH SuperHプロセッサのアーキテクチャ This book is intended for engineers, and explains in detail the architecture of SuperH microprocessors from the basics. It covers the differences from single-chip microprocessors, such as cache and MMU, development environment, and driver programming for on-chip peripheral components. Ohmsha Link to external site
Book SuperH SuperHで学ぶμIRTON仕様OS -リアルタイムOSの動作原理と実装法がわかる!- This book explains the necessity of real-time OS, introduces the functions of the μITRON OS, and explains actual coding and task scheduling using plenty of examples and figures. This book can be used as an introduction to learning to build systems using μITRON OS. Dempa Shimbun Link to external site
Book SuperH SH-3&SH-4プロセッサ入門 This book covers the features of the SuperH Family and an overview of the newest CPU core SH-4A, as well as the basic way to use SH-3 and SH-4 and examples of initialization, use of peripheral functions, and so on. CQ Publishing Link to external site
Book SuperH SH-1&SH-2マイコン入門 This book covers the features of the SuperH Family and an overview of the newest CPU core SH-2A, as well as the basic way to use SH-1 and SH-2 and application examples of DTC, ATU, and Ether controller. CQ Publishing Link to external site

Link to external site
Book SuperH これならわかるSuperHマイコン This book covers the knowledge required for programming the Renesas embedded RISC SuperH Family (both microcontrollers and microprocessors) in C. It presents effective ways of using FPU and DSP coprocessors, exception handling, and cache memory, and ways to increase development efficiency for software engineers. This book explains basics such as the instructions and internal configuration of SuperH MCUs and MPUs in an easy-to-understand way, and introduces application examples using internal and external peripheral functions. Ohmsha Link to external site
Book SuperH SH-2マイコンで学ぶ組み込み開発入門 This book explains hardware configuration, programming methods, use cases, and more using an SH-2 microcontroller (SH7144) as an example. CQ Publishing Link to external site
Book 78K, R8C, H8 マイコンと表示器をつなぐ10の方法 This book contains examples of display device (LED or LCD) control using 78K, R8C, and H8 microcontrollers. CQ Publishing Link to external site
Book 78K USBマイコンでパソコンI/O![78K0基板付き] This book comes with a 78K0 microcontroller board equipped with a USB interface. Simply by plugging this 78K0 board into the USB port of a personal computer, you can program and transfer data. You can learn about the USB function of the 78K0 using an actual board. CQ Publishing Link to external site
Book R8C R8C/Tinyマイコン・リファレンス・ブック This book covers in detail the features of the CPU core and effective ways of using it, and how to use the peripheral functions that are built into the R8C/14 to R8C/17 devices. CQ Publishing

Link to external site

Link to external site

Book R8C 電子工作のためのR8C/Tinyスタートアップ This book explains R8C/Tiny architecture, functions, development environment, and example projects in detail. CQ Publishing Link to external site
Book R8C すぐに使える! 実験・試作用マイコン・モジュール This book, introduces an R8C microcontroller module, essential points when using an R8C microcontroller, and an example of an application. The example application is a practical example of the creation of a PC-linked application in Visual Basic on a PC. CQ Publishing Link to external site
Book H8 H8マイコンによる組込み制御・プログラムの基礎を理解 マイコン入門講座 This book is a well-balanced introduction to the basics of principles of operation of microcontrollers, memory, and programming, using H8 microcontrollers as examples. The reader can learn and understand basics of computer programming that will continue to be valuable, such as the concepts of microcontroller system configuration and CPU, binary numbers, and assembly language. Dempa Shimbun Link to external site
Book H8 H8マイコン+C言語効率アップテクニック This book covers techniques for improving the efficiency of H8 microcontroller programs written in C. It explains a variety of methods for improving efficiency, such as through the specifications of the C language, microcontroller factors, and optimizing the development environment. Ohmsha Link to external site
Book H8 C言語でH8マイコンを使いこなす This book explains the knowledge necessary for mastering H8 microcontrollers in an easy-to-understand way, focusing on specific control methods using embedded C programming. Ohmsha Link to external site
Book H8 H8マイコン完全マニュアル This book explains the basics of how to use H8 microcontrollers and applications in an easy-to-understand way. Ohmsha Link to external site
Book H8 ラダー図によるH8マイコン活用入門 This book uses the Renshi ladder compiler, which generates a microcontroller execution program from a ladder diagram, to explain methods of utilizing microcontroller systems. The bundled CD-ROM contains Renshi Standard, which supports the H8/3694F and can generate MOT files for programming from ladder diagrams. CQ Publishing Link to external site
Book H8 H8/Tinyマイコン完璧マニュアル This book covers everything from programming basics to application techniques, using the H8/3694F. CQ Publishing Link to external site
Book H8 組み込みマイコン教科書 H8 I/O編 This book covers many C programing examples using the H8/3052. In addition to the control of peripheral functions such as interrupt handling and DMA, motor control methods are also explained in detail. CQ Publishing Link to external site
Book H8 はじめてのH8マイコン This book can be used to learn programming that uses a line trace robot using H8 microcontrollers. CQ Publishing Link to external site
Book H8 ぼくらのマイコン・ロボット工作 This book describes the building of three types of robots using H8 Tiny microcontrollers. Starting from principles of robotic control, the peripheral circuitry of motors and sensors and software creation methods are also covered. CQ Publishing Link to external site
Magazine Other Design Wave Magazine 2004年 10月号 This volume contains an article on an example of memory-saving development using TCP/IP protocol stack (Part 2). CQ Publishing Link to external site
Magazine Other Design Wave Magazine 2004年 9月号 This volume contains an article on an example of memory-saving development using TCP/IP protocol stack (Part 1). CQ Publishing Link to external site
Book Other 組込みマイコンで学ぶCANプロトコルとプログラミング CAN入門講座 CAN (Controller Area Network) is a serial communications protocol for automotive electronics that was developed with the goal of reducing the weight of vehicles. Now, it has evolved even further, and is employed in many fields, including factory automation, industrial equipment, medical equipment, and marine vessels. This book explains the specifications of the CAN standard and how to use it using examples of usage by actual microcontrollers (contains CAN control programs using the M16C, H8 and SuperH microcontrollers). Dempa Shimbun Link to external site
Magazine Other Interface 2008年 2月号 トラブらない,バグらない組み込み製品開発技法 Trouble-free, bug-free embedded product development technique CQ Publishing Link to external site
Magazine Other Interface 2005年 8月号 TCP/IP+Ethernet ネットワーク機器設計法 TCP/IP + Ethernet network device design CQ Publishing Link to external site
Book Other グリーンエレクトロニクス No.1 内容: R2A20121SP を使う…大電力・高電力密度に対応フェーズ  シフト・フル・ ブリッジ ZVS電源の設計と試作 Contents: Using the R2A20121SP - Phase Shift Full Bridge ZVS Power Supply Design and Prototyping for Large Power and High Power Density CQ Publishing Link to external site
Book Other グリーンエレクトロニクス No.2 内容: DALI/DMX512規格で自在にコントロール LED照明/イルミネーションを制御するための通信 Contents: Full control using DALI/DMX512 standards; communications for LED lighting/illumination control. CQ Publishing Link to external site
Book Other グリーンエレクトロニクス No.3 内容:R2A20114を使いSiC-SBDとIGBTを駆動 インターリーブ連続モード3kW PFCの設計と試作 Contents: SiC-SBD and IGBT Drive Using the R2A20114 - Interleaved Continuous Conduction Mode 3kW PFC Design and Prototyping CQ Publishing Link to external site
Book Other グリーンエレクトロニクス No.5 内容:電力をコンデンサに貯めてマイコンで無線通信 数Wの太陽電池を活用したセンサ・ネットワーク・モジュールの試作 Contents: Storing electric power to a capacitor and performing wireless communication using a microcontroller; prototyping of a sensor network module using a solar battery of several watts CQ Publishing Link to external site
Book Other グリーンエレクトロニクス No.12 This volume contains a special feature on digitally control power supply design using Renesas microcontrollers. CQ Publishing Link to external site
Magazine Other トランジスタ技術 2008年5月号 内容: 1.5 kW の低ノイズ高調波対策電源を作れる 臨界モード/インターリーブPFC IC R2A20112 Contents: Creating a 1.5 kW Low-Noise Power Supply with High Harmonic Suppression - The R2A20112 Critical Conduction Mode/Interleaving PFC IC CQ Publishing Link to external site
Book Other 組込みシステム概論 This book covers the current state of embedded system development, real examples of embedded systems for digital cameras and automatic ticket gates, embedded system design and development procedures, and embedded system hardware and software technology. CQ Publishing Link to external site

Chinese

Cover Type Category Title Summary Publisher Related Information
Book V850 Automotive Electronics Embedded system development and application(V850) Mainly for automotive application development basic knowledge, focus in CAN, self-programming, RTOS development in automotive system. Includes C and assembly language reference codes. Modern Education Press (MEP) (现代教育出版社) Link to external site
Book 78K Embedded SYSTEM development based on MCU (78K0) For MCU beginners to learn MCU basic knowledge and skill for development, with sample of IO, PWM, Timer, Serial Interface, A/D application. Economy & Management Publishing House (经济管理出版社) Link to external site
Book 78K MCU application and training for electronic design contest(78K0) High level application training with 8bit MCU for students who want to join electronic design contest. Especially in LCD display and DC motor, step motor control. Economy & Management Publishing House (经济管理出版社) Link to external site
Book R8C RENESAS R8C/1A,1B MCU theory and application Basic introduction and training for RENESAS 8-Bit MCU R8C/1A,1B. For MCU beginners. Tsinghua University Press (清华大学出版社) Amazon.cn
Book R8C Renesas R8C/11 MCU theory and application Written by Renesas's engineers for MCU education and development mainly. Tsinghua University Press (清华大学出版社) Amazon.cn
Book M16C RENESAS M16C/62 Embedded MCU program design Introduces M16C/62 program design technology with M16C/62 development board. This book is for education and reference for new engineers. Huazhong University of Science & Technology Press (华中科技大学出版社) Link to external site
Book M16C Mitsubishi M16C/62 MCU theory and application Written by Tsinghua University's professor and Renesas's engineer for MCU education and development mainly. Beihang University Press (北京航空航天大学出版社) Link to external site
Book M16C Renesas M16C/62P MCU theory and application Written by Renesas's engineers for MCU education and development mainly. Tsinghua University Press (清华大学出版社) Amazon.cn
Book H8-SLP RENESAS H8-SLP MCU theory and application Basic introduction and training for RENESAS 8-Bit MCU H8-SLP. For MCU beginners. Tsinghua University Press (清华大学出版社) Link to external site
Book 7544 RENESAS 7544 MCU theory and application Basic introduction and training for RENESAS 7544 MCU For MCU beginners. Tsinghua University Press (清华大学出版社) Amazon.cn

Brazilian Portuguese

*A My Renesas ID is required for downloading the PDFs.

Cover Type Category Title Summary Publisher Related Information PDF
Book RL78 Microcontroladores RL78 Guia Básico Um guia prático sobre
microcontroladores de alto desempenho e daixo consumo de energia para
sistemas embarcados
Renesas Books  

Download*

Menu
Contact